cancel
Showing results for 
Search instead for 
Did you mean: 

STML432KC: CAN Bootloader functionality

godlyblade
Associate III

Refer to AN2606 p. 260 - 263

There it says, that for STM32L43xxx derivatives CAN1 bootloader is mapped to PB8 pin (RX) and PB9 pin (TX). My derivative supports CAN but doesn't have these pins, because of a 32 Pin package. Is there a possibility to use the CAN Bootloader anyway?

Best Regards!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Uwe Bonnes
Chief

There is no way to use the system CAN Bootloader when you do not have the pins.

View solution in original post

2 REPLIES 2
Uwe Bonnes
Chief

There is no way to use the system CAN Bootloader when you do not have the pins.

godlyblade
Associate III

Okay, thanks!