2021-03-30 6:00 AM
Hi
Can anyone please show me an example of a working USB CDC Host sending the SetControlLineState command? This hasn't been implemented in the STM32 HAL drivers/middleware but it should be a simple thing to add.
SetControlLineState is used to signal the Host is ready to receive data from the CDC device. I tried adding and calling my own routine after the USB enumeration completes:
USBH_StatusTypeDef USBH_CDC_SetControlLineState(USBH_HandleTypeDef *phost)
{
phost->Control.setup.b.bmRequestType = USB_H2D | USB_REQ_TYPE_CLASS | USB_REQ_RECIPIENT_INTERFACE;
phost->Control.setup.b.bRequest = CDC_SET_CONTROL_LINE_STATE;
phost->Control.setup.b.wValue.w = 3U;
phost->Control.setup.b.wIndex.w = 2;
phost->Control.setup.b.wLength.w = 0;
return USBH_CtlReq(phost, 0, 0);
}
The transmitted data appears to be correctly formed but the phost->RequestState appears to get stuck on CMD_WAIT expecting a reply from the device which I understand is not part of the CDC protocol. I then modified USBH_CtlReq to always set phost->RequestState = CMD_SEND when called from the above procedure but I still cannot get the USB CDC device to send data out.
I would be gratedul for a working USB CDC Host SetControlLineState example or suggestions to try.
Thank you in advance.
2021-12-13 6:41 AM
Hi ST,
I am waiting as well for exaktly the same feature or I am looking for a way to set the DTR signal on an USB device.
2025-01-27 12:50 PM
Was there any solution to this?
I am using the STM32407 discovery board in USB CDC Host mode and am trying to communicate with another MCU in USB CDC ACM Device mode. The other MCU works fine when connecting to a PC and can see that the DTR signal is being sent.
I am not sure how to do this on the STM32 side since it is not implemented in the stack?