cancel
Showing results for 
Search instead for 
Did you mean: 

UART_WaitOnFlagUntilTimeout

Kai_Satone
Senior

i was debugging code HAL_uart_Receive ();

sprintf(command, "AT+CMGL=\"ALL\"\r\n");//read all sms HAL_UART_Transmit(&huart1, (uint8_t *)command, strlen(command), 10); // HAL_Delay(100); HAL_UART_Receive(&huart1, RXbuffer, sizeof(RXbuffer), HAL_MAX_DELAY);

 i jump suddenly in here

/** * @brief This function handles UART Communication Timeout. It waits * until a flag is no longer in the specified status. * @PAram huart Pointer to a UART_HandleTypeDef structure that contains * the configuration information for the specified UART module. * @PAram Flag specifies the UART flag to check. * @PAram Status The actual Flag status (SET or RESET). * @PAram Tickstart Tick start value * @PAram Timeout Timeout duration * @retval HAL status */ static HAL_StatusTypeDef UART_WaitOnFlagUntilTimeout(UART_HandleTypeDef *huart, uint32_t Flag, FlagStatus Status, uint32_t Tickstart, uint32_t Timeout) { /* Wait until flag is set */ while ((__HAL_UART_GET_FLAG(huart, Flag) ? SET : RESET) == Status) { /* Check for the Timeout */ if (Timeout != HAL_MAX_DELAY) { if (((HAL_GetTick() - Tickstart) > Timeout) || (Timeout == 0U)) { return HAL_TIMEOUT; } if ((READ_BIT(huart->Instance->CR1, USART_CR1_RE) != 0U) && (Flag != UART_FLAG_TXE) && (Flag != UART_FLAG_TC)) { if (__HAL_UART_GET_FLAG(huart, UART_FLAG_ORE) == SET) { /* Clear Overrun Error flag*/ __HAL_UART_CLEAR_OREFLAG(huart); /* Blocking error : transfer is aborted Set the UART state ready to be able to start again the process, Disable Rx Interrupts if ongoing */ UART_EndRxTransfer(huart); huart->ErrorCode = HAL_UART_ERROR_ORE; /* Process Unlocked */ __HAL_UNLOCK(huart); return HAL_ERROR; } } } } return HAL_OK; }
View more


how to solve this problem?

6 REPLIES 6
Karl Yamashita
Principal

That's not a problem because that's what you've instructed the HAL driver to do.

You've used HAL_MAX_DELAY which is waiting for ~49 days before it returns from the timeout or you've received the correct amount of bytes.

Replace HAL_MAX_DELAY to something like 100, which will return after 100ms timeout. 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

Still same problem

It's supposed to go to that function. So you need to explain in more detail what YOU think is the problem.

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

while running 

sprintf(command, "ATE1\r\n"); HAL_UART_Transmit(&huart1, (uint8_t *)command, strlen(command), 10); HAL_UART_Receive(&huart1, buffer, sizeof(buffer), 100); memset(command, 0, sizeof(command)); sprintf(command, "AT+CMGF=1\r\n");//text mode HAL_UART_Transmit(&huart1, (uint8_t *)command, strlen(command), 10); HAL_UART_Receive(&huart1, buffer, sizeof(buffer), 200); memset(command, 0, sizeof(command)); sprintf(command, "AT+CPMS=\"SM\",\"SM\",\"SM\"\r\n"); HAL_UART_Transmit(&huart1, (uint8_t *)command, strlen(command), 10); HAL_UART_Receive(&huart1, buffer, sizeof(buffer), 100); sscanf(buffer, "%*[^:]:%d", &num_sms); // MAX_SENTENCES = num_sms; if (num_sms == 0) { return; } memset(command, 0, sizeof(command));

code 

it struck into below code

/** * @brief This function handles UART Communication Timeout. It waits * until a flag is no longer in the specified status. * @PAram huart Pointer to a UART_HandleTypeDef structure that contains * the configuration information for the specified UART module. * @PAram Flag specifies the UART flag to check. * @PAram Status The actual Flag status (SET or RESET). * @PAram Tickstart Tick start value * @PAram Timeout Timeout duration * @retval HAL status */ static HAL_StatusTypeDef UART_WaitOnFlagUntilTimeout(UART_HandleTypeDef *huart, uint32_t Flag, FlagStatus Status, uint32_t Tickstart, uint32_t Timeout) { /* Wait until flag is set */ while ((__HAL_UART_GET_FLAG(huart, Flag) ? SET : RESET) == Status) { /* Check for the Timeout */ if (Timeout != HAL_MAX_DELAY) { if (((HAL_GetTick() - Tickstart) > Timeout) || (Timeout == 0U)) { return HAL_TIMEOUT; } if ((READ_BIT(huart->Instance->CR1, USART_CR1_RE) != 0U) && (Flag != UART_FLAG_TXE) && (Flag != UART_FLAG_TC)) { if (__HAL_UART_GET_FLAG(huart, UART_FLAG_ORE) == SET) { /* Clear Overrun Error flag*/ __HAL_UART_CLEAR_OREFLAG(huart); /* Blocking error : transfer is aborted Set the UART state ready to be able to start again the process, Disable Rx Interrupts if ongoing */ UART_EndRxTransfer(huart); huart->ErrorCode = HAL_UART_ERROR_ORE; /* Process Unlocked */ __HAL_UNLOCK(huart); return HAL_ERROR; } } } } return HAL_OK; }
View more

 

Ok, so now we know the problem. You should have said you're stuck in that function the first place, instead of only saying "i jump suddenly in here".

 

Sounds like the System Tick is not working. 

Make sure you've have it selected

KarlYamashita_1-1726308609356.png

And that the NVIC is correct

KarlYamashita_2-1726308966878.png

 

 

If you do have it selected, then try debugging. In the stm32f4xx_it.c file, place a breakpoint on the HAL_IncTick and run in debug mode. 

KarlYamashita_0-1726308372505.png

 

If it doesn't break on you breakpoint, then maybe it's a clock issue? 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

Thank you sir,
same  thing we have done as you told we have put up break point on it

Kai_Satone_2-1726833817069.png

while debugging mode after HAL_Delay(100);
we stuck on 

void SysTick_Handler(void) { /* USER CODE BEGIN SysTick_IRQn 0 */ /* USER CODE END SysTick_IRQn 0 */ HAL_IncTick(); /* USER CODE BEGIN SysTick_IRQn 1 */ /* USER CODE END SysTick_IRQn 1 */ }

here.
can you please guide me what's solution