2024-09-12 4:57 AM
i was debugging code HAL_uart_Receive ();
sprintf(command, "AT+CMGL=\"ALL\"\r\n");//read all sms
HAL_UART_Transmit(&huart1, (uint8_t *)command, strlen(command), 10);
// HAL_Delay(100);
HAL_UART_Receive(&huart1, RXbuffer, sizeof(RXbuffer), HAL_MAX_DELAY);
i jump suddenly in here
/**
* @brief This function handles UART Communication Timeout. It waits
* until a flag is no longer in the specified status.
* @PAram huart Pointer to a UART_HandleTypeDef structure that contains
* the configuration information for the specified UART module.
* @PAram Flag specifies the UART flag to check.
* @PAram Status The actual Flag status (SET or RESET).
* @PAram Tickstart Tick start value
* @PAram Timeout Timeout duration
* @retval HAL status
*/
static HAL_StatusTypeDef UART_WaitOnFlagUntilTimeout(UART_HandleTypeDef *huart, uint32_t Flag, FlagStatus Status,
uint32_t Tickstart, uint32_t Timeout)
{
/* Wait until flag is set */
while ((__HAL_UART_GET_FLAG(huart, Flag) ? SET : RESET) == Status)
{
/* Check for the Timeout */
if (Timeout != HAL_MAX_DELAY)
{
if (((HAL_GetTick() - Tickstart) > Timeout) || (Timeout == 0U))
{
return HAL_TIMEOUT;
}
if ((READ_BIT(huart->Instance->CR1, USART_CR1_RE) != 0U) && (Flag != UART_FLAG_TXE) && (Flag != UART_FLAG_TC))
{
if (__HAL_UART_GET_FLAG(huart, UART_FLAG_ORE) == SET)
{
/* Clear Overrun Error flag*/
__HAL_UART_CLEAR_OREFLAG(huart);
/* Blocking error : transfer is aborted
Set the UART state ready to be able to start again the process,
Disable Rx Interrupts if ongoing */
UART_EndRxTransfer(huart);
huart->ErrorCode = HAL_UART_ERROR_ORE;
/* Process Unlocked */
__HAL_UNLOCK(huart);
return HAL_ERROR;
}
}
}
}
return HAL_OK;
}
how to solve this problem?
2024-09-12 4:46 PM
That's not a problem because that's what you've instructed the HAL driver to do.
You've used HAL_MAX_DELAY which is waiting for ~49 days before it returns from the timeout or you've received the correct amount of bytes.
Replace HAL_MAX_DELAY to something like 100, which will return after 100ms timeout.
2024-09-13 1:28 AM
Still same problem
2024-09-13 7:41 AM
It's supposed to go to that function. So you need to explain in more detail what YOU think is the problem.
2024-09-13 11:42 PM
while running
sprintf(command, "ATE1\r\n");
HAL_UART_Transmit(&huart1, (uint8_t *)command, strlen(command), 10);
HAL_UART_Receive(&huart1, buffer, sizeof(buffer), 100);
memset(command, 0, sizeof(command));
sprintf(command, "AT+CMGF=1\r\n");//text mode
HAL_UART_Transmit(&huart1, (uint8_t *)command, strlen(command), 10);
HAL_UART_Receive(&huart1, buffer, sizeof(buffer), 200);
memset(command, 0, sizeof(command));
sprintf(command, "AT+CPMS=\"SM\",\"SM\",\"SM\"\r\n");
HAL_UART_Transmit(&huart1, (uint8_t *)command, strlen(command), 10);
HAL_UART_Receive(&huart1, buffer, sizeof(buffer), 100);
sscanf(buffer, "%*[^:]:%d", &num_sms);
// MAX_SENTENCES = num_sms;
if (num_sms == 0)
{
return;
}
memset(command, 0, sizeof(command));
code
it struck into below code
/**
* @brief This function handles UART Communication Timeout. It waits
* until a flag is no longer in the specified status.
* @PAram huart Pointer to a UART_HandleTypeDef structure that contains
* the configuration information for the specified UART module.
* @PAram Flag specifies the UART flag to check.
* @PAram Status The actual Flag status (SET or RESET).
* @PAram Tickstart Tick start value
* @PAram Timeout Timeout duration
* @retval HAL status
*/
static HAL_StatusTypeDef UART_WaitOnFlagUntilTimeout(UART_HandleTypeDef *huart, uint32_t Flag, FlagStatus Status,
uint32_t Tickstart, uint32_t Timeout)
{
/* Wait until flag is set */
while ((__HAL_UART_GET_FLAG(huart, Flag) ? SET : RESET) == Status)
{
/* Check for the Timeout */
if (Timeout != HAL_MAX_DELAY)
{
if (((HAL_GetTick() - Tickstart) > Timeout) || (Timeout == 0U))
{
return HAL_TIMEOUT;
}
if ((READ_BIT(huart->Instance->CR1, USART_CR1_RE) != 0U) && (Flag != UART_FLAG_TXE) && (Flag != UART_FLAG_TC))
{
if (__HAL_UART_GET_FLAG(huart, UART_FLAG_ORE) == SET)
{
/* Clear Overrun Error flag*/
__HAL_UART_CLEAR_OREFLAG(huart);
/* Blocking error : transfer is aborted
Set the UART state ready to be able to start again the process,
Disable Rx Interrupts if ongoing */
UART_EndRxTransfer(huart);
huart->ErrorCode = HAL_UART_ERROR_ORE;
/* Process Unlocked */
__HAL_UNLOCK(huart);
return HAL_ERROR;
}
}
}
}
return HAL_OK;
}
2024-09-14 3:17 AM
Ok, so now we know the problem. You should have said you're stuck in that function the first place, instead of only saying "i jump suddenly in here".
Sounds like the System Tick is not working.
Make sure you've have it selected
And that the NVIC is correct
If you do have it selected, then try debugging. In the stm32f4xx_it.c file, place a breakpoint on the HAL_IncTick and run in debug mode.
If it doesn't break on you breakpoint, then maybe it's a clock issue?
2024-09-20 5:07 AM
Thank you sir,
same thing we have done as you told we have put up break point on it
while debugging mode after HAL_Delay(100);
we stuck on
void SysTick_Handler(void)
{
/* USER CODE BEGIN SysTick_IRQn 0 */
/* USER CODE END SysTick_IRQn 0 */
HAL_IncTick();
/* USER CODE BEGIN SysTick_IRQn 1 */
/* USER CODE END SysTick_IRQn 1 */
}
here.
can you please guide me what's solution