cancel
Showing results for 
Search instead for 
Did you mean: 

Trouble with uart reception in nucleo144-stm32f746

jack focker
Associate II
Posted on April 09, 2017 at 08:13

Hi dear friends,

I have a problem with uart reception.

I can't receive any data or maybe i can't init it correctly.

I assign gpio to it and init it according to user manual. it has transmission but no data can receive. I don't no why??

Can everybody show me an example?

I used example of uart in stm32cubef7 too , but no reception can be done.

#stm32 #uart #stm32f746-nucleo #cubef7
13 REPLIES 13
Posted on April 10, 2017 at 18:53

This worked for me on the F767ZI

0690X00000603fmQAA.jpg

https://drive.google.com/open?id=0B7OY5pub_GfITEtjaDhzM1BnVVk

 

And F746ZG, same .HEX

0690X00000603kGQAQ.jpg
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on April 11, 2017 at 02:41

If it is not apparent, the F7 goes into USART echo mode once it has output the diagnostic info, ie any thing you type at the terminal at 115200 8N1 is echoed back as received. Seems to be functioning as designed.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on April 11, 2017 at 03:19

What's the name of the register that has the ram size?

Posted on April 11, 2017 at 05:23

RAM size has been inferred from the FLASH size described in System ROM

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..