2025-02-05 02:52 PM
While recenting working on the FLASH peripheral for F2-F4-F7 devices (as their structure is pretty close), I noticed a few differences between the reference manuals and the device SVD. I'm not sure who's right and who's wrong in this situation (although I would tend to consider the RMs more reliable), but it would be great if both sources could be more coherent.
So here's the list for each register (non exhaustive, there may be some I haven't seen):
There are probably variants of the mentioned MCU that I haven't checked but that are certainly affected by the same problems.
Thanks for taking this into consideration !
2025-02-05 11:43 PM - edited 2025-02-06 02:32 AM
Hello @vinchatl ,
Thank you for having reported this!
I am checking it internally and I will come-back to you with updates (internal ticket 202427)
(PS: Internal ticket number 202427 is not accessible or usable by customers)