2018-12-15 3:25 AM
DS, RM and Nucleo-boards are already available, but I couldn't find a SVD file for the G0 series.
Solved! Go to Solution.
2018-12-17 5:58 AM
Hello @Andreas Bolsch ,
The SVD file is available under the Keil pack STM32G0xx_DFP.1.0.0.pack, you can download it from Keil (http://www.keil.com/dd2/pack/#/eula-container)
The pack version can be obtain, as well, into Project->Manage->Pack Installer : right side -> Packs tab, select "Device Specific", and expand "Keil::STM32G0xx_DFP".
Kind Regards,
Imen
2018-12-17 5:58 AM
Hello @Andreas Bolsch ,
The SVD file is available under the Keil pack STM32G0xx_DFP.1.0.0.pack, you can download it from Keil (http://www.keil.com/dd2/pack/#/eula-container)
The pack version can be obtain, as well, into Project->Manage->Pack Installer : right side -> Packs tab, select "Device Specific", and expand "Keil::STM32G0xx_DFP".
Kind Regards,
Imen
2018-12-19 12:27 PM
MDK 5.27pre is now available for download http://www2.keil.com/mdk5/
STM32G0 Packs listed, updates for most other STM32 lines
2020-11-19 8:26 AM
Hi @Andreas Bolsch
As my colleague mentioned, the SVD files are a part of the keil pack.
Nevertheless, soon the SVD file for STM32G0 series will be published as a stand alone file on the ST website.
I will notify you once it is official.
Thank you for your feedback!
-Imen
2020-12-29 7:30 AM
Hi,
Just an update!
SVD files for STM32G0 series have been officially posted on ST web site and available via this link under the System View Description section.
regards,
-Imen