cancel
Showing results for 
Search instead for 
Did you mean: 

SVD errors on STM32H503

hijax_pl
Associate II

Using python I have written small app to convert SVD V1.4 into assembly include. Then I started to write assemby code using RM0492 Rev2 .

For the peripherals I use (RCC,ADC,GPIO,GPDMA,TIM,USART) I have found that there are few errors in the SVD file, some typos etc.

Namely:

RCC_CCIPR5 register has only 2 fields described, no info about FDCANSEL, DACSEL & ADCDACSEL

RCC_CFGR regsiter shall be named RCC_CFGR1

For RCC_PLL1CFGR & RCC_PLL2CFGR there are DIVMx while should be PLLxM

 

 

 

2 REPLIES 2
STTwo-32
ST Employee

Hello @hijax_pl 

Thank you for repoorting those typos. I'm escalating the second and the third points as they are for correction. But the first point, i find that we have a typo only on the name and discription of the bit values for DACSEL.They others looks fine on my side.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Yes, my mistake.

I have filtered out DAC & FDCAN as peripherals but also from RCC defines.

And yes, DACSEL is DAC1SEL in reference manual.