2024-11-23 7:05 AM
Using python I have written small app to convert SVD V1.4 into assembly include. Then I started to write assemby code using RM0492 Rev2 .
For the peripherals I use (RCC,ADC,GPIO,GPDMA,TIM,USART) I have found that there are few errors in the SVD file, some typos etc.
Namely:
RCC_CCIPR5 register has only 2 fields described, no info about FDCANSEL, DACSEL & ADCDACSEL
RCC_CFGR regsiter shall be named RCC_CFGR1
For RCC_PLL1CFGR & RCC_PLL2CFGR there are DIVMx while should be PLLxM
2024-11-23 8:44 AM - edited 2024-12-05 8:36 AM
Hello @hijax_pl
Thank you for reporting those typos. I'm escalating the second and the third points as they are for correction (under internal ticket number 197881). But the first point, I find that we have a typo only on the name and description of the bit values for DACSEL. They others looks fine on my side.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-23 10:26 AM
Yes, my mistake.
I have filtered out DAC & FDCAN as peripherals but also from RCC defines.
And yes, DACSEL is DAC1SEL in reference manual.
2024-11-24 11:06 AM
Do not know if I shall open new thread but anyway.
(1) Why TIM1_SMCR and TIM2/3_SMCR have different naming convetions for SMS / TS fields?
i.e. for TIM1_SMCR there are SMS/SMS_1 and TS/TS_1 and for TIM2/3_SMCR, SMS1/SMS2 and TS1/TS2 respectively.
(2) Also TIM1_SMCR_TS_1 field has no enumerated values, while for TIM2/3_SMCR_TS2 there are, but wrongly described. TIM1_SMCR_TS & TIM2/3_SMCR_TS1 has enums for the range 0..7 only, ie. the TS1 field itself.
As in the RM those fields must be combined, I think the easies way forward would be to provide enums only for the TS1 field, and add missing values:
B_0x10000:Internal Trigger 4 (tim_itr4)
B_0x10001:Internal Trigger 5 (tim_itr5)
B_0x10002:Internal Trigger 6 (tim_itr6)
B_0x10003:Internal Trigger 7 (tim_itr7)
B_0x10004:Internal Trigger 8 (tim_itr8)
B_0x10005:Internal Trigger 9 (tim_itr9)
B_0x10006:Internal Trigger 10 (tim_itr10)
B_0x10007: Internal trigger 11 (tim_itr11)
B_0x20000: Internal trigger 12 (tim_itr12)
B_0x20001: Internal trigger 13 (tim_itr13)
B_0x20002: Internal trigger 14 (tim_itr14)
B_0x20003: Internal trigger 15 (tim_itr15)
(and repeat that pattern for all other fields that are splitted acrose registers)
Then one can code by just shifting the chosen enum to the TS1 field position.
2024-11-24 11:33 AM
And this time: ADC_CFGR register and EXTSEL field.
In SVD this single field is split among four 1-bit long ones (according to RM0492) and enumerated values desciptions are messed up (adc_ext_trg0 & adc_ext_trg1 repeated for all 4 "subfields")
RM0492 discusses this as single field, which is correct, i.e.
"Bits 9:5 EXTSEL[4:0]: External trigger selection for regular group
These bits select the external event used to trigger the start of conversion of a regular group:
00000: adc_ext_trg0
00001: adc_ext_trg1
00010: adc_ext_trg2
00011: adc_ext_trg3
00100: adc_ext_trg4
00101: adc_ext_trg5
00110: adc_ext_trg6
00111: adc_ext_trg7
...
11111: adc_ext_trg31"
etc...
Is SVD created from RM or vice versa? Either way I think both RM0492 (page 579) and SVD shall be corrected.