2025-07-24 2:40 AM - last edited on 2025-07-24 3:00 AM by Andrew Neil
Hello,
I have a STM32U585CIUA and generate a PWM with 125Hz 2ms high and 6ms low phase on TIM1 on PA2.
I would like to start another PWM with TIM2 50Khz 1us high and 19us low on the falling edge of PA2, which is then stopped after 200 cycles.
In all my setting attempts, however, TIM2 starts before TIM no matter how it is configured and even if I set the HAL for TIM2 after TIM1 in the code...
Can anyone help me with this?
Dave
static void MX_TIM1_Init(void)
{
/* USER CODE BEGIN TIM1_Init 0 */
/* USER CODE END TIM1_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
/* USER CODE BEGIN TIM1_Init 1 */
/* USER CODE END TIM1_Init 1 */
htim1.Instance = TIM1;
htim1.Init.Prescaler = 319;
htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
htim1.Init.Period = 3999;
htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim1.Init.RepetitionCounter = 0;
htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_Init(&htim1) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_OC1REF;
sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_OC1REF;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 1000;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
sBreakDeadTimeConfig.DeadTime = 0;
sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;
sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;
sBreakDeadTimeConfig.BreakFilter = 0;
sBreakDeadTimeConfig.BreakAFMode = TIM_BREAK_AFMODE_INPUT;
sBreakDeadTimeConfig.Break2State = TIM_BREAK2_DISABLE;
sBreakDeadTimeConfig.Break2Polarity = TIM_BREAK2POLARITY_HIGH;
sBreakDeadTimeConfig.Break2Filter = 0;
sBreakDeadTimeConfig.Break2AFMode = TIM_BREAK_AFMODE_INPUT;
sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM1_Init 2 */
/* USER CODE END TIM1_Init 2 */
HAL_TIM_MspPostInit(&htim1);
}
/**
* @brief TIM2 Initialization Function
* None
* @retval None
*/
static void MX_TIM2_Init(void)
{
/* USER CODE BEGIN TIM2_Init 0 */
/* USER CODE END TIM2_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_SlaveConfigTypeDef sSlaveConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
/* USER CODE BEGIN TIM2_Init 1 */
/* USER CODE END TIM2_Init 1 */
htim2.Instance = TIM2;
htim2.Init.Prescaler = 159;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 19;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sSlaveConfig.SlaveMode = TIM_SLAVEMODE_RESET;
sSlaveConfig.InputTrigger = TIM_TS_ITR2;
if (HAL_TIM_SlaveConfigSynchro(&htim2, &sSlaveConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 1;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM2_Init 2 */
/* USER CODE END TIM2_Init 2 */
HAL_TIM_MspPostInit(&htim2);
}
2025-07-24 6:06 AM
I don't see any code actually starting the timers.
You could set one timer as a slave that gets started when the first timer starts.
2025-07-24 6:37 AM - edited 2025-07-24 6:39 AM
Hi,
attached function hows start the PWM's...
No matter what I do or set, Timer 2 always starts first... :(
void LEDDecay_CaptureAndAverage(void)
{
// 1) Summen-Puffer löschen
for (uint16_t i = 0; i < DECAY_POINTS; i++) {
sumBuffer[i] = 0;
}
for (uint8_t rep = 0; rep < DECAY_REPEATS; rep++) {
decayDone = false;
// 2) LEDs via TIM1-PWM einschalten (erster OC1REF → TRGO2)
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_11, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_SET);
HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);
// 3) TIM2 als Slave-Reset & Sampling starten
__HAL_TIM_SET_COUNTER(&htim2, 0);
HAL_TIM_Base_Start(&htim2);
HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_3); // Debug-Puls auf PA2
// 4) ADC1 + DMA starten (200 Samples via TIM2_TRGO)
HAL_ADC_Start_DMA(&hadc1, (uint32_t*)decayBuffer, DECAY_POINTS);
// 5) Warten auf DMA-Complete
while (!decayDone) {
__WFI();
}
decayDone = false;
// 6) Cleanup nach Messreihe
HAL_ADC_Stop_DMA(&hadc1);
HAL_TIM_PWM_Stop(&htim2, TIM_CHANNEL_3);
HAL_TIM_Base_Stop(&htim2);
HAL_TIM_PWM_Stop(&htim1, TIM_CHANNEL_1);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_11, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_RESET);
// 7) Werte aufsummieren
for (uint16_t i = 0; i < DECAY_POINTS; i++) {
sumBuffer[i] += decayBuffer[i];
}
}
// 8) Durchschnitt berechnen
for (uint16_t i = 0; i < DECAY_POINTS; i++) {
avgBuffer[i] = (uint16_t)(sumBuffer[i] / DECAY_REPEATS);
}
decayDone = true;
}Hi
2025-07-25 2:58 AM
You need to call HAL_TIM_Base_Start(&htim1) before HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1).
2025-07-29 2:35 AM
Hello @ProNet36
Did you check this example below ?