cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4 UL safety Flash memory complete check sum self test failed, checksum is not generating in the Atollic IDE please help me

NPULI.1
Associate II

i am working on STM32L4 STL Safety Libraries checking FLASH CRC using Atollic true studio , Here the IDE not generating checksum please suggest me what are configuration need to in the IDE, how to verify flash test ?

Control Flow Error (main loop, Flash CRC)

1 REPLY 1
DamienF
Associate II

in my context the CRC table is generated and appended to the image post-build via a command line call to the STM32CubeProgrammer.

Example:

STM32_Programmer_CLI.exe sl- "$PROJ_DIR$\myproj\Exe\Project.out‘’ 0x8000000 0x08200000 0x400