User Activity

What I'd like to ask on this community forum is, has anyone faced any issue integrating the STL library? An FAE is engaged on this issue, with no response as of yet. We have good overall success, with the exception of the TM12 module, which fails occ...
We are integrating the STL library in the context of a project requiring IEC 61508 safety integrity level 2 (SIL2). How can we programmatically pull the version info out of the STL library? The API doesn't show anything to that effect. Also, what's t...
The STL library is configured to test a multiple of sectors at a time (128kByte each).Our usage model is closely derived from the Nucleo reference project that ST provides as an aid to integrate the STL library; and we're using the IAR project in tha...