cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7xx Option Bytes Bug & Cube HAL Flash OB_IWDG_SW definition

Ernest Lotter
Associate II

ISSUE 1 :

------------

User option byte IWDG1_SW in register FLASH_OPTSR[4] not working correctly with uVision V5.28.0.0 (MDK-ARM Essential).

Problem description:

After settings the user option byte IWDG1_SW = 0, to indicate HW start of Independent Watchdog I cannot load the image anymore using Keil.

The erase and program sequence start and progresses unusually quickly to:

Erase Done.

Programming Done.

Followed by many lines of:

Contents mismatch at: 08000000H (Flash=00H Required=88H) !

Contents mismatch at: 08000001H (Flash=00H Required=24H) !

...

And then

Too many errors to display !

Flash Load finished at ...

NOTE: Sometimes the problem is a different complaint related to memory access.

This issue happens regardless of settings the IWDG1_SW = 0 in code or from ST link utility.

Only the ST link utility manage to reflash the unit in this state, but usually only after unit manual reset.

Setup:

  • STM32H743BITx MCU
  • Vision V5.28.0.0 (MDK-ARM Essential)
  • Debugger: ULink Pro Cortex Debugger or ST Link/V2
  • Changing from Option Byte factory defaults to OB_IWDG_HW

ISSUE 2 :

------------

Keil::STM32H7xx_DFP V2.5.0 (2020-03-23) file stm32h7xx_hal_flash_ex.h incorrectly defines

#define OB_IWDG_SW      0x20U /*!< Software IWDG selected */ AND

#define OB_WWDG_SW    0x10U /*!< Software WWDG selected */

This does not match the reference manual which indicates IWDG1_SW bit in register FLASH_OPTSR to be in position 4 (0x10U). This is confirmed also by the mask FLASH_OPTSR_IWDG1_SW which has value 0x10U.

Furthermore, not sure why definition OB_WWDG_SW and macro IS_OB_WWDG_SOURCE is defined, because it is not an option to enable with option byte?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee

Hi @Ernest Lotter​ ,

I'll try to reproduce and check Issue 1, then will keep you informed.

Regarding Issue 2: please note that stm32h7xx_hal_flash_ex.h was updated. Now we define: OB_IWDG1_SW, OB_IWDG1_HW, OB_IWDG2_SW and OB_IWDG2_HW.

This was done because in STM32H7 dual-core devices we have 2 IWDGs.

However, it remains wrong to define OB_WWDG_SW and OB_WWDG_HW. A request is tracked internally to remove them.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.