cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32H750B-DK TouchGFX + FreeRTOS + LWIP Ping not working ?

lhwa .1
Associate II

Hello, im inquiring after thinking about it for a few days.
please help me.
this is my dev environment 
CMSIS_V2
TouchGFX designer : 4.22
CubeMX : 6.9.0
CubeIDE : 1.13.1
DevKIT : Stm32H750B-DK
i want to do a ping test on this board
i ran it with reference to this example, but it doesn't work.
(https://github.com/GrzHeller/STM32H750B-DK_TouchGFX_FreeRTOS_MQTT_Example)
i don't know what the problem is.

lhwa1_0-1691370129638.png

lhwa1_1-1691370165467.png

lhwa1_2-1691370211620.png

Please help me 

Thank you

 

4 REPLIES 4
KDJEM.1
ST Employee

Hello @lhwa .1 ,

I advise you to start by configuring the LWIP. For that I recommend you to follow the steps shared in this FAQ How do I create a project for STM32H7 with Ethernet and LwIP stack working?.

The Goal of this example is to:

  • Configure project in STM32CubeMX for STM32H750-Discovery
  • Configure FreeRTOS and LwIP middlewares correctly
  • Send UDP message periodically (optional)

I hope this help you!

Thank you.

Kaouthar


To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

thankyou your reply

i tested thing 

ping test OK

UDP Server/Client OK

TCP NG : Assertion "pbuf_free: p->ref > 0" failed at line 753

i don't know why the reason about a week 

 

JJhin.1
Senior II

In IP address setting give for PC's address in default getway . And try again