cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743 ADC clock configuration

PStor
Associate

In RM 0433 on page 910 there is the following:

“1. The ADC clock can be a specific clock source, named adc_ker_ck_input which is

independent and asynchronous with the AHB clock.

It can be configured in the RCC (refer to RCC Section for more information on how to

generate the ADC clock (adc_ker_ck_input) dedicated clock).�?

 I didn’t find any information about configuring asynchronous ADC clock in RCC.  Information in   UM2217 explains only how to divide ADC asynchronous clock.

Please explain how is it possible to configure the asynchronous ADC clock in RCC using HAL or LL.

2 REPLIES 2

0690X000008aH9yQAE.png

JW

PStor
Associate

Good picture , but what about severel strings of code with ADC clock configuration ?