2021-09-25 12:22 AM
I use STM32H723VET6. Bootloader ver 9.2. When I can send command GO at FDCAN (PD1, PD0), I receive ACK(0x79), but after that MCU is fail.
My function:
void BootCanGo(uint8_t* answer)
{
uint32_t Delayer = 0x8FFFFF;
uint8_t SendedData[4];
CanTxHeader.Identifier = BOOT_CAN_COMMAND_GO;
SendedData[0] = 0x08;
SendedData[1] = 0x00;
SendedData[2] = 0x00;
SendedData[3] = 0x00;
/* Start the Transmission process */
CanTxHeader.DataLength = FDCAN_DLC_BYTES_4;
HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan, &CanTxHeader, SendedData);
while ((HAL_FDCAN_GetRxFifoFillLevel(&hfdcan, FDCAN_RX_FIFO0) < 1) && --Delayer) {};
HAL_FDCAN_GetRxMessage(&hfdcan, FDCAN_RX_FIFO0, &CanRxHeader, CanRxData);
*answer = CanRxData[0];
}
Write memory and Erase memory commands run correct. A program in flash memory mode (BOOT0 pin LOW) run correct. There are no limitations in AN2606:
I tried to run the debugger on the STM32H723 (device side). I stop the program, and after the command GO I start it again in step mode. After of several steps disconnection occurs:
Flash in STM32H723:
What am I doing wrong?
2021-10-01 8:35 AM
Hello @BLeon.2 ,and welcome to the Community,
Make sure to properly configure the vector table.
Do you use/enable interrupts? Did you try with BOOT0 in high?
Imen
2021-10-01 9:14 AM
Vector Tables, Watchdog, Stacks, Interrupts, expectations.
Have code very early in Reset_Handler (in assembler) assert/toggle GPIO or tweet/squawk via UART. Confirm it's entering your code, and then check-point from there on out..
Have HardFault_Handler() and Error_Handler() that report actionable data, not die silently.
2021-10-01 10:00 AM
The address of the entry to the main() does not appear in the PC register. Failure occurs in system memory. I checked the VTOR register through CubeProgrammer (0xE000ED08), turned on disable interrupts in main program, nothing helped.
2021-10-01 10:14 AM
main() is significant down-stream from the Reset_Handler, SystemInit, and initialization of statics, etc.
Start at the point that transfer of control occurs, figure out who's dying. If the ROM's handed-off to you, it's role is over.
2021-10-01 11:36 AM
Above in the line of the disambler:
-> 0x1FF1274E F7FFF9B4 BL.W 0x1FF11ABA
there is a write the address of the next instruction to LR: 0x1FF1ABA, which does not exist.
2021-10-01 12:07 PM
I think you're wrong on the details/interpretation, suggest you save a copy of the Loader ROM, and send/attach that here.
2021-10-01 12:38 PM
2021-10-01 1:00 PM
1FF11ABA SUB16 sub_1FF11ABA: ; Xref 1FF1274E
1FF11ABA E92D 4FF8 stmdb sp!, {r3, r4, r5, r6, r7, r8, r9, r10, r11, lr}
1FF11ABE 2000 movs r0, #0
1FF11AC0 F8DF 446C ldr.w r4, [pc, #1132] ; $1FF11F30=$24002D04
1FF11AC4 9000 str r0, [sp, #0]
1FF11AC6 F20F 4874 addw r8, pc, #1140 ; $474
1FF11ACA F88D 0000 strb.w r0, [sp]
1FF11ACE F44F 3900 mov.w r9, #131072 ; $20000
1FF11AD2 F8DF 7460 ldr.w r7, [pc, #1120] ; $1FF11F34=$24002904
1FF11AD6 F44F 3580 mov.w r5, #65536 ; $10000
1FF11ADA F8DF 6450 ldr.w r6, [pc, #1104] ; $1FF11F2C=$24001868
1FF11ADE F8DF A444 ldr.w r10, [pc, #1092] ; $1FF11F24=$240035A0
1FF11AE2 E016 b.n loc_1FF11B12
1FF11AE4 LOC loc_1FF11AE4: ; Xref 1FF11B50
1FF11AE4 6030 str r0, [r6, #0]
1FF11AE6 2079 movs r0, #121
1FF11AE8 60F5 str r5, [r6, #12]
1FF11AEA 463A mov r2, r7
1FF11AEC 7038 strb r0, [r7, #0]
1FF11AEE 4631 mov r1, r6
1FF11AF0 4650 mov r0, r10
1FF11AF2 F7FF FD2A bl sub_1FF1154A
1FF11AF6 60F5 str r5, [r6, #12]
1FF11AF8 2010 movs r0, #16
1FF11AFA F000 F8C1 bl sub_1FF11C80
1FF11AFE F8C6 900C str.w r9, [r6, #12]
1FF11B02 2000 movs r0, #0
1FF11B04 8038 strh r0, [r7, #0]
1FF11B06 LOC loc_1FF11B06: ; Xref 1FF11BC2
1FF11B06 F000 F8BC bl sub_1FF11C82
1FF11B0A 60F5 str r5, [r6, #12]
1FF11B0C 2079 movs r0, #121
1FF11B0E LOC loc_1FF11B0E: ; Xref 1FF11BFA 1FF11C7E
1FF11B0E F000 F8B7 bl sub_1FF11C80
1FF11B12 LOC loc_1FF11B12: ; Xref 1FF11AE2 1FF11B1C 1FF11B86 1FF11BC8
1FF11B12 ; 1FF11BF4 1FF11C00 1FF11C06 1FF11C28
1FF11B12 2140 movs r1, #64
1FF11B14 4650 mov r0, r10
..
1FF12734 LOC loc_1FF12734: ; Xref 1FF12734 1FF12740 1FF12746 1FF1274C
1FF12734 ; 1FF12752
1FF12734 E7FE b.n loc_1FF12734
1FF12736 LOC loc_1FF12736: ; Xref 1FF12724
1FF12736 F8DF 1588 ldr.w r1, [pc, #1416] ; $1FF12CC0=$240037B8
1FF1273A 6008 str r0, [r1, #0]
1FF1273C F7FA FD9D bl sub_1FF0D27A
1FF12740 E7F8 b.n loc_1FF12734
1FF12742 LOC loc_1FF12742: ; Xref 1FF12728
1FF12742 F7FD FFB4 bl sub_1FF106AE
1FF12746 E7F5 b.n loc_1FF12734
1FF12748 LOC loc_1FF12748: ; Xref 1FF12720
1FF12748 F7FF FF96 bl sub_1FF12678
1FF1274C E7F2 b.n loc_1FF12734
1FF1274E LOC loc_1FF1274E: ; Xref 1FF1272C
1FF1274E F7FF F9B4 bl sub_1FF11ABA
1FF12752 E7EF b.n loc_1FF12734
1FF12754 LOC loc_1FF12754: ; Xref 1FF1272E
1FF12754 F3BF 8F4F dsb sy
1FF12758 F8DF 1568 ldr.w r1, [pc, #1384] ; $1FF12CC4=$E000ED0C
1FF1275C F8DF 0568 ldr.w r0, [pc, #1384] ; $1FF12CC8=$05FA0004
1FF12760 680A ldr r2, [r1, #0]
1FF12762 F402 62E0 and.w r2, r2, #1792 ; $700
1FF12766 4302 orrs r2, r0
1FF12768 600A str r2, [r1, #0]
1FF1276A F3BF 8F4F dsb sy
1FF1276E LOC loc_1FF1276E: ; Xref 1FF12770
1FF1276E BF00 nop
1FF12770 E7FD b.n loc_1FF1276E
...
2021-10-01 1:30 PM
1FF11BCA LOC loc_1FF11BCA_cmd_21_go: ; Xref 1FF11B5C
1FF11BCA 6030 str r0, [r6, #0]
1FF11BCC F000 F98E bl sub_1FF11EEC
1FF11BD0 4683 mov r11, r0
1FF11BD2 F1BB 3F55 cmp.w r11, #1431655765 ; $55555555
1FF11BD6 D00E beq.n loc_1FF11BF6
1FF11BD8 F000 F858 bl sub_1FF11C8C
1FF11BDC 4658 mov r0, r11
1FF11BDE F7FC F849 bl sub_1FF0DC74
1FF11BE2 2803 cmp r0, #3
1FF11BE4 BF18 it ne
1FF11BE6 2802 cmp r0, #2
1FF11BE8 D105 bne.n loc_1FF11BF6
1FF11BEA F000 F84F bl sub_1FF11C8C
1FF11BEE 4658 mov r0, r11
1FF11BF0 F7FC FA0D bl sub_1FF0E00E_GoCode
1FF11BF4 E78D b.n loc_1FF11B12
1FF0E00E SUB16 sub_1FF0E00E_GoCode: ; Xref 1FF0D46C 1FF107E2 1FF11BF0 1FF126A4
1FF0E00E ; 1FF13084
1FF0E00E B538 push {r3, r4, r5, lr}
1FF0E010 4604 mov r4, r0
1FF0E012 F000 F93E bl sub_1FF0E292
1FF0E016 F7FF FFF7 bl sub_1FF0E008_InterruptEnable
1FF0E01A 1D20 adds r0, r4, #4
1FF0E01C 6805 ldr r5, [r0, #0]
1FF0E01E 6820 ldr r0, [r4, #0]
1FF0E020 F7FF FFEA bl sub_1FF0DFF8_LoadMSP
1FF0E024 47A8 blx r5
1FF0E026 BD31 pop {r0, r4, r5, pc}