cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 swap problem

Sridhar
Associate II

I am facing difficulty in making bank swapping example code to work, provided in STM32Cube_FW_H7_V1.8.0.

I had tried the following options

  1. I had flashed the "FLASH_SwapBank_Bank1.bin" and "FLASH_SwapBank_Bank2.bin" file onto the respective banks and observed that only the respective bank LED is toggling.
  2. I had created two projects respectively for each bank along with the linker files and flashed both the .bin files and observed that only the respective bank LED is toggling.

In both the above cases bank swapping is not happening.

I am attaching the main files and the linker files. can any one guide me, if any mistake is made in these.

Linker file changes Bank 1

/* Memories definition */

MEMORY

{

 DTCMRAM  (xrw)  : ORIGIN = 0x20000000,  LENGTH = 128K

 ITCMRAM  (xrw)  : ORIGIN = 0x00000000,  LENGTH = 64K

 RAM_D1  (xrw)  : ORIGIN = 0x24000000,  LENGTH = 512K

 RAM_D2  (xrw)  : ORIGIN = 0x30000000,  LENGTH = 288K

 RAM_D3  (xrw)  : ORIGIN = 0x38000000,  LENGTH = 64K

 FLASH  (rx)  : ORIGIN = 0x8000000,  LENGTH = 1024K

}

Bank 2

/* Specify the memory areas */

MEMORY

{

DTCMRAM (xrw)   : ORIGIN = 0x20000000, LENGTH = 128K

RAM_D1 (xrw)   : ORIGIN = 0x24000000, LENGTH = 512K

RAM_D2 (xrw)   : ORIGIN = 0x30000000, LENGTH = 288K

RAM_D3 (xrw)   : ORIGIN = 0x38000000, LENGTH = 64K

ITCMRAM (xrw)   : ORIGIN = 0x00000000, LENGTH = 64K

FLASH (rx)   : ORIGIN = 0x8100000, LENGTH = 1024K

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0