Hello everybody.
I have problems with uarts in the my bootloader. In the main program the communication works OK.
The client card is stm32g484 based.
The first problem:
After HAL_NVIC_SystemReset()from main app enter to bootloader and HAL_UART_Transmit() send data to host but host received nothing. HAL_UART_Transmit() returns HAL_OK but the sniffer received nothing.
The second problem:
50-70% of the times the bootloader stopped accepting the data after erasing the flash. The next time (power cycle) the program will work fine.
------------------------------------------------------------------
int main(void)
{
int16_t pack_left = 1, data_size;
uint32_t pack_offset;
flash_status status = FLASH_OK;
HAL_StatusTypeDef hal_status; //grom 21feb2024 vA1
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
__enable_irq();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_IWDG_Init();
HAL_IWDG_Refresh(&hiwdg);
LoadComConfig();
HAL_IWDG_Refresh(&hiwdg);
MX_LPUART1_UART_Init(UARTs.Uart4.BaudRate);
MX_USART1_UART_Init(UARTs.Uart1.BaudRate);
MX_USART2_UART_Init(UARTs.Uart2.BaudRate);
MX_USART3_UART_Init(UARTs.Uart3.BaudRate);
HAL_UART_Receive_DMA(&hlpuart1, buffer4, ENTER_COUNT);
HAL_UART_Receive_DMA(&huart1, buffer1, ENTER_COUNT);
HAL_UART_Receive_DMA(&huart2, buffer2, ENTER_COUNT);
HAL_UART_Receive_DMA(&huart3, buffer3, ENTER_COUNT);
uint32_t tickstart = HAL_GetTick();
while (
((HAL_UART_GetState(&huart1) != HAL_UART_STATE_READY)
|| (HAL_UART_GetState(&huart2) != HAL_UART_STATE_READY)
|| (HAL_UART_GetState(&huart3) != HAL_UART_STATE_READY)
|| (HAL_UART_GetState(&hlpuart1) != HAL_UART_STATE_READY))
&& ((HAL_GetTick() - tickstart) < BL_UART_DELAY))
{
HAL_IWDG_Refresh(&hiwdg);
}
uint8_t is_ok = 0;
if (HAL_UART_GetState(&huart1) == HAL_UART_STATE_READY)
{
for (int i = 0; i < ENTER_COUNT; i++)
{
if (buffer1[i] == ENTER_CHAR)
is_ok++;
}
huart = &huart1;
buffer = buffer1;
}
else if (HAL_UART_GetState(&huart2) == HAL_UART_STATE_READY)
{
for (int i = 0; i < ENTER_COUNT; i++)
{
if (buffer2[i] == ENTER_CHAR)
is_ok++;
}
huart = &huart2;
buffer = buffer2;
}
else if (HAL_UART_GetState(&huart3) == HAL_UART_STATE_READY)
{
for (int i = 0; i < ENTER_COUNT; i++)
{
if (buffer3[i] == ENTER_CHAR)
is_ok++;
}
huart = &huart3;
buffer = buffer3;
}
else if (HAL_UART_GetState(&hlpuart1) == HAL_UART_STATE_READY)
{
for (int i = 0; i < ENTER_COUNT; i++)
{
if (buffer3[i] == ENTER_CHAR)
is_ok++;
}
huart = &hlpuart1;
buffer = buffer4;
}
HAL_UART_DMAStop(&huart1);
__HAL_DMA_DISABLE_IT(&hdma_usart1_rx, (DMA_IT_TC | DMA_IT_HT | DMA_IT_TE));
HAL_DMA_DeInit(huart1.hdmarx);
HAL_UART_DMAStop(&huart2);
__HAL_DMA_DISABLE_IT(&hdma_usart2_rx, (DMA_IT_TC | DMA_IT_HT | DMA_IT_TE));
HAL_DMA_DeInit(huart2.hdmarx);
HAL_UART_DMAStop(&huart3);
__HAL_DMA_DISABLE_IT(&hdma_usart3_rx, (DMA_IT_TC | DMA_IT_HT | DMA_IT_TE));
HAL_DMA_DeInit(huart3.hdmarx);
HAL_UART_DMAStop(&hlpuart1);
__HAL_DMA_DISABLE_IT(&hdma_lpuart1_rx, (DMA_IT_TC | DMA_IT_HT | DMA_IT_TE));
HAL_DMA_DeInit(hlpuart1.hdmarx);
if (is_ok == ENTER_COUNT)
{
/*
* start package update
*/
tx_data[0] = (uint8_t)VERSION;
HAL_UART_Transmit(huart, tx_data, 1, HAL_MAX_DELAY);
/*
* flash erase
*/
for (uint32_t i = FLASH_APP_START_PAGE; i < FLASH_APP_END_PAGE; i++)
{
status = Flash_Erase(i, 1);
tx_data[0] = (uint8_t)status;
HAL_IWDG_Refresh(&hiwdg);
HAL_Delay(50);
if (status != FLASH_OK)
{
HAL_UART_Transmit(huart, tx_data, 1, HAL_MAX_DELAY);
Error_Handler(); //error
}
}
HAL_UART_Transmit(huart, tx_data, 1, HAL_MAX_DELAY);
/*
* write to flash
*/
do
{
uint8_t sum = 0;
/*
* start byte
*/
do
{
hal_status = HAL_UART_Receive(huart, buffer, 1, 100000);
if (hal_status != HAL_OK)
{
tx_data[0] = (uint8_t)COM_ERROR;
HAL_UART_Transmit(huart, tx_data, 1, HAL_MAX_DELAY);
Error_Handler();
}
HAL_IWDG_Refresh(&hiwdg);
} while (buffer[0] != START_CHAR);
sum = buffer[0];
/*
* read package header
*/
hal_status = HAL_UART_Receive(huart, buffer, MESSAGE_HEADER, 100000);
if (hal_status != HAL_OK)
{
tx_data[0] = (uint8_t)COM_ERROR;
HAL_UART_Transmit(huart, tx_data, 1, HAL_MAX_DELAY);
Error_Handler();
}
HAL_IWDG_Refresh(&hiwdg);
/*
* unpacking the package
*/
//Pack Offset
((uint8_t*)&pack_offset)[0] = buffer[0];
((uint8_t*)&pack_offset)[1] = buffer[1];
((uint8_t*)&pack_offset)[2] = buffer[2];
((uint8_t*)&pack_offset)[3] = buffer[3];
if ((pack_offset & 0x08) != 0)
{
//offset error
tx_data[0] = (uint8_t)DATA_OFFSET_ERROR;
HAL_UART_Transmit(huart, tx_data, 1, HAL_MAX_DELAY);
Error_Handler(); //error
}
//Pack left
((uint8_t*)&pack_left)[0] = buffer[4];
((uint8_t*)&pack_left)[1] = buffer[5];
//Data size
((uint8_t*)&data_size)[0] = buffer[6];
((uint8_t*)&data_size)[1] = buffer[7];
for (int8_t i = 0; i < MESSAGE_HEADER; i++)
{
sum += buffer[i];
}
HAL_IWDG_Refresh(&hiwdg);
/*
* read data
*/
hal_status = HAL_UART_Receive(huart, buffer, data_size + 1, 100000);
if (hal_status != HAL_OK)
{
tx_data[0] = (uint8_t)COM_ERROR;
HAL_UART_Transmit(huart, tx_data, 1, HAL_MAX_DELAY);
Error_Handler();
}
HAL_IWDG_Refresh(&hiwdg);
for (int i = 0; i < data_size; i++)
{
sum += buffer[i];
}
/*
* check CS
*/
if (sum != buffer[data_size])
{
//CS error
tx_data[0] = (uint8_t)COM_ERROR_CS;
HAL_UART_Transmit(huart, tx_data, 1, HAL_MAX_DELAY);
Error_Handler(); //error
}
if ((data_size & 0b0111) != 0) //if (mod(data_size,8))
{
if (pack_left != 0)
{
tx_data[0] = (uint8_t)DATA_SIZE_ERROR;
HAL_UART_Transmit(huart, tx_data, 1, HAL_MAX_DELAY);
Error_Handler(); //error
}
else
{
//fill to 64bit
for (int i = 0; i < 8; i++)
tx_data[data_size + i] = 0xff;
data_size = (data_size + & 0xfff8;
}
}
HAL_IWDG_Refresh(&hiwdg);
//write to flash
status = Flash_Write(FLASH_APP_START_ADDRESS + pack_offset, (uint64_t *)buffer, data_size);
tx_data[0] = (uint8_t)status;
HAL_UART_Transmit(huart, tx_data, 1, HAL_MAX_DELAY);
if (status != FLASH_OK)
Error_Handler(); //error
} while (pack_left != 0);
}
//go to main project
HAL_UART_DeInit(&huart1);
HAL_UART_DeInit(&huart2);
HAL_UART_DeInit(&huart3);
HAL_RCC_DeInit();
HAL_DeInit();
__disable_irq();
extern void* _app_start[];
SCB->VTOR = _app_start;
((void(*)())_app_start[1])();
}
-----------------------------
static void MX_LPUART1_UART_Init(uint32_t BaudRate)
{
hlpuart1.Instance = LPUART1;
hlpuart1.Init.BaudRate = BaudRate;
hlpuart1.Init.WordLength = UART_WORDLENGTH_8B;
hlpuart1.Init.StopBits = UART_STOPBITS_1;
hlpuart1.Init.Parity = UART_PARITY_NONE;
hlpuart1.Init.Mode = UART_MODE_TX_RX;
hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
hlpuart1.Init.ClockPrescaler = UART_PRESCALER_DIV10; //UART_PRESCALER_DIV1;
hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&hlpuart1) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&hlpuart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&hlpuart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&hlpuart1) != HAL_OK)
{
Error_Handler();
}
}
---------------------------
initializing of usart1,usart2,usart3 it same
---------------------------
static void MX_USART1_UART_Init(uint32_t BaudRate)
{
huart1.Instance = USART1;
huart1.Init.BaudRate = BaudRate;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart1) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&huart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&huart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&huart1) != HAL_OK)
{
Error_Handler();
}
}