cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G474RE: Trying to port AN5305 example to NUCLEO-G474RE board

Manu Abraham
Senior

Hi Folks,

Need a bit help in trying to figure out what's going on.

I have been trying to port the

en.stm32cubeg4_v1-2-0\STM32Cube_FW_G4_V1.2.0\Projects\B-G474E-DPOW1\Examples\FMAC

FMAC_Buck_VoltageMode_HW_AN5305

to a

NUCLEO-G474RE platform.

I am trying to observe HRTIM TC1. TC2 waveforms on the NUCLEO-G474RE board.

AFAICS, the difference between the NUCLEO-G474RE and the B-G474E-DPOW1 is the lack of a Joystick and the MOSFET's. Is the example a fully working example, any thoughts ?

(Maybe it has some issue to run on the NUCLEO board, ..)

I wondered at least I could monitor the waveforms on the NUCLEO board. but the example does not seem to run/generate any waveforms.

Kind of clueless, digging through the HAL code as to why the example wouldn't generate the HRTIM waveform on the NUCLEO board.

Is there something that i am missing ?

Thanks,

Manu

0 REPLIES 0