STM32G431KB; Fatal problem with USB initialization function
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-18 10:18 PM
FreeRTOS is currently active. However, the problem occurs before FreeRTOS initialization (before calling osKernelInitialize ()).
​
The board used is a board written by hand rather than a NUCLEO board. When I activate my Peripheral devices other than USB-PD and run the FreeRTOS application, I confirm that it works correctly.
​
The point where the problem occurs is inside the USB_DisableGlobalInt function. In the process of masking the interrupt mask to USBx-> CNTR, all interrupts are immediately interrupted (including the SWD of ST-LINK) and the chip is reset after a certain time.
​
Here is the call stack at the time of occurrence:
[0] from 0x08004b88 in USB_DisableGlobalInt+0 at Drivers/STM32G4xx_HAL_Driver/Src/stm32g4xx_ll_usb.c:117
[1] from 0x08004aa0 in HAL_PCD_Init+28 at Drivers/STM32G4xx_HAL_Driver/Src/stm32g4xx_hal_pcd.c:169
[2] from 0x08000908 in MX_USB_PCD_Init+32 at Src/main.c:483
[3] from 0x080009b2 in main+34 at Src/main.c:122
​
The code for each call stack is as follows:
[0]
106 HAL_StatusTypeDef USB_DisableGlobalInt(USB_TypeDef *USBx)
107 {
108 uint16_t winterruptmask;
109
110 /* Set winterruptmask variable */
111 winterruptmask = USB_CNTR_CTRM | USB_CNTR_WKUPM |
112 USB_CNTR_SUSPM | USB_CNTR_ERRM |
113 USB_CNTR_SOFM | USB_CNTR_ESOFM |
114 USB_CNTR_RESETM | USB_CNTR_L1REQM;
115
116 /* Clear interrupt mask */
117 USBx->CNTR &= ~winterruptmask; // << Stucks at this point
118
119 return HAL_OK;
120 }
[1]
154 {
155 hpcd->MspInitCallback = HAL_PCD_MspInit;
156 }
157
158 /* Init the low level hardware */
159 hpcd->MspInitCallback(hpcd);
160 #else
161 /* Init the low level hardware : GPIO, CLOCK, NVIC... */
162 HAL_PCD_MspInit(hpcd);
163 #endif /* (USE_HAL_PCD_REGISTER_CALLBACKS) */
164 }
165
166 hpcd->State = HAL_PCD_STATE_BUSY;
167
168 /* Disable the Interrupts */
169 __HAL_PCD_DISABLE(hpcd); // <<< Stucks At This Point
170
171 /* Init endpoints structures */
172 for (i = 0U; i < hpcd->Init.dev_endpoints; i++)
173 {
[2]
475 hpcd_USB_FS.Instance = USB;
476 hpcd_USB_FS.Init.dev_endpoints = 8;
477 hpcd_USB_FS.Init.speed = PCD_SPEED_FULL;
478 hpcd_USB_FS.Init.phy_itface = PCD_PHY_EMBEDDED;
479 hpcd_USB_FS.Init.Sof_enable = DISABLE;
480 hpcd_USB_FS.Init.low_power_enable = DISABLE;
481 hpcd_USB_FS.Init.lpm_enable = DISABLE;
482 hpcd_USB_FS.Init.battery_charging_enable = DISABLE;
483 if (HAL_PCD_Init(&hpcd_USB_FS) != HAL_OK) // << Stucks at this point
484 {
​
I don't know if this is a known issue, but I couldn't find it when I tried searching on Google.
​
Please let me know if there is any additional information you need to solve the problem, such as board configuration or CubeMX settings.
​
Thanks.​
​
Solved! Go to Solution.
- Labels:
-
STM32CubeMX
-
STM32G4 Series
-
USB-PD
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-19 8:50 AM
> The error was resolved when I switched clock source to HSI ...
So it was missing clock to USB?
But, you've said above,
> It is set to use HSI48,.
So how is it?
For crystal capacitors see AN2867, but generally 22pF for 24MHz should be in most of the cases OK and the oscillator should work, even if not optimally. Check HSE oscillations by outputting it to MCO and measuring there.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-19 1:00 AM
Check, whethr USB clock is enabled in RCC.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-19 1:41 AM
I've checked clock configuration. It is set to use HSI48, instead of PLLQ, since PLLQ is can't be set to 48MHz by adjusting PLL parameters, when the SysClk is set to 170MHz. Should I use PLLQ, despite of reducing SysClk speed as multiplicand of 48MHz?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-19 2:47 AM
I guess, any clock source is OK for the initial setup - the USB data transmittion may not work properly with an incorrect frequency source, but reset etc. should work.
My question was more that check whether RCC_APB1ENR1.USBEN is set.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-19 5:13 AM
Yes, when I evaluate below expression, it returns 1.
(RCC->APB1ENR1 & RCC_APB1ENR1_USBEN) != 0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-19 6:39 AM
Single-step in disasm. Show line where the "freeze" occurs, together with context (previous lines, content of registers).
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-19 6:47 AM
I'm using gdb-dashboard, you'll may recognize statement easily with images.
Program runs properly before branch into the function USB_DisableGlobalInt()
Right after jump into this function, it seems working properly.
Yet if I step one instruction on this statement, connection immediately shutdown and freezes.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-19 6:49 AM
Oops, sorry, Image was not uploaded ... Plz see next comment
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-19 6:55 AM
(Click to see)
[1]
[2]
After above statement, the system does not respond anymore; freezes.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-19 7:14 AM
Since the program freezes as soon as the pc enters the function USB_DisableGlobalInt(), I have inserted several meaningless volatile instructions as a test in front-side of the function. However, it still freezes as soon as jumping into this function, even before executes them.
It seems like the function call itself freezes the program.