2019-04-08 12:40 PM
We have a design using the STM32F778. The FS USB works fine with VDD = 3.3V. When VDD = 1.8V, the USB does not work. VDDUSB is connected to 3.3V in both cases. On some boards, the FS USB will be detected by PC as a bootloader but it does not actually work. Anyone have success with one of the STM32F7 parts USB when VDD = 1.8V?
2019-04-09 9:46 AM
Hello,
Check the condition in this datasheet relevant to your device.
Regards,
Imen.
2019-04-09 9:54 AM
Check the power sequences to follow. Maybe the power up/down is wrong.
2019-04-09 10:03 AM
The power sequence is compatible with what is in the datasheet.
2019-04-09 2:26 PM
What is your max HCLK when using Vdd=1.8?
2019-04-09 4:49 PM
180 MHz