User Activity

Hi,Setup:https://github.com/Open-CMSIS-Pack/STM32U5xx_DFP/blob/main/CMSIS/Debug/STM32U535_545_575_585_59x_5Ax.dbgconfCompiler: ARM Keil MDKv5 version 5.41When using Embedded Trace (Sync Trace with 4-bit) and the Debug Description file (.dbgconf Confi...
Hi,I'm developing a new application for the STM32U5A5 processor. The application runs correctly if I program (flash) and debug with the JTAG/SWD debugger. Even after disconnecting the debugger, the application still runs, and it is possible to re-pro...
Posted on March 22, 2018 at 21:56Hi, We are evaluating the use of the BT Module SPBT3.0DP1 on one of our devices.We are trying to configure the PIN to connect to a legacy device, that already has a predetermined PIN code that uses letters (lower and...