2021-01-08 06:55 AM
Dear all,
first I have to say that I am new to STM32F7 mirocontrollers, but I am not new to ARM-Cortex M4/M7 based controllers in general, nor the lwIP stack nor FreeRTOS.
I have the following two problems:
My application from the first question is configured like the LwIP_HTTP_Server_Netconn_RTOS example (MPU, fixed sections in memory), as far as I can reengineer it from the LwIP_HTTP_Server_Netconn_RTOS source files.
Kind regards and thank you for your help.
Solved! Go to Solution.
2021-01-23 11:39 AM
Hi @wastl
the build issue is reproduced, identified and solved:
open the project settings and edit the preporcessor include path shown in the screen shot, it has invisible extra spaces at the end which is causing the build problem.
remove the extra spaces and the issue will disappear.
try to run the application an let us know 😉
regards
Haithem.
2021-01-23 12:21 PM
Hi @Haithem Rahmani ,
compiling the example works now, thanks for the tip.
Unfortunately, I still can not ping the board. I connected it to my Fritz.box to test DHCP, but the DHCP server can not assign an IP address (application then gets the static IP address 192.169.0.10). I also connected the Nucleo board directly to my notebook, configured my network card with 192.168.0.9 and tried to ping the Nucleo board - no success.
The ping response given by the board is the same as in my code, still contains a lot of 0x55 octets. I attached a screenshot, ping request is line 39, the reply given by the Nucleo board is line 40, the data section is also shown in the screenshot.
I think I am going to order a new board (just to be sure, the board is not that expensive) and some other "interesting stuff" to avoid the shipping costs.
Kind regards.
Wastl
2021-01-23 12:46 PM
Hi @Haithem Rahmani ,
thanks for the tip, the project compiles now without problems.
Unfortunately, I still can not ping the board. I tried two setups:
Find attached a screenshot of the Wireshark capture of setup 2 (ping request line 39, response line 40 e.g.). As you can see, the data section still contains a lot 0x55 octets.
However, I think I am going to order a second board (it is not that expensive) with some other "interesting stuff" to avoid the shipping costs ;-).
Kind regards.
wastl
2021-01-29 01:29 PM
Dear @Haithem Rahmani ,
today my new Nucleo-F767ZI board arrived.
For a first test, I just flashed the LwIP_HTTP_Server_Netconn_RTOS example and tried to ping the board (IP address 192.168.0.10 and see there... It works!!! I don't know why but it seems to be an hardware related issue with my old board. However, further tests with my application are not done yet, I will let you know about the results.
Kind regards.
Wastl
2021-01-29 10:22 PM
great news!
just to let you know, the AzureRTOS is available on github for the STM32H7 it comes with a full featured TCP/IP stack the NetXDuo.
it supports the STM32H723Nucleo-ZG it is worth trying 🙂
regards
Haithem.
2021-01-30 02:43 AM
Dear @Haithem Rahmani ,
my FreeRTOS + lwIP application also works. As I did not change anything in the code, I would say that it can be confirmed that my first Nucleo-Board has a hardware issue.
Thanks for the help.
By the way: Is there a button (or something else) to mark my problem as resolved?
Kind regards.
Sebastian Reichhold
2021-01-30 03:00 AM
@Imen DAHMEN could you please update this post as resolved?
regards
Haithem.
2021-01-30 05:01 AM
> However, I tried this example here... but even this example does not work.
As everything, that firmware also is not absolutely perfect and has some issues. After some time I will update it to even better performing and more polished one. 🙂 That said, the issues are minor and not a showstoppers. It's probably useful to try with another network equipment and DHCP server just to be sure. Does the new board work in same conditions?
> Is there a button (or something else) to mark my problem as resolved?
Press "Select as Best" under the specific post.
2021-01-30 05:18 AM
I do not expect the firmware to be perfect ;-). My problem was that I could debug the signals the whole way from the microcontroller memory to the PHY and I could not find anything wrong. That is why I decided to order the new board to exclude a hardware problem on the old board.
I just tried the new board with the LwIP_HTTP_Server_Netconn_RTOS example, getting the IP address via a DHCP server (still my Fritz.Box). Worked very well, there were no problems pinging the board or visiting the webserver site with a browser (Firefox).
So I guess there is a hardware problem with the old board.
I marked my post with the result that there most likely is a hardware problem with the old board as "Select as Best".
Regards.