Skip to main content
MGogr.1
Senior
September 21, 2024
Solved

TCP Client Raw API

  • September 21, 2024
  • 3 replies
  • 2197 views

Hello,

I have STM32F767ZI and STM32F429ZI Nucleo board, which I want to configure in TCP Client mode. I have attached .ioc file and tcpclient.c and ethernetif.c files. This files I have downloaded from internet. Now here is my problem when I try to run this code my board is not getting connected to server. For server I am using Hercules software. My board/s are getting from ping response, but not getting connected to server.

 

 

 

void tcp_echoclient_connect(void)
{
 ip_addr_t DestIPaddr;
 
 /* create new tcp pcb */
 echoclient_pcb = tcp_new();
 
 if (echoclient_pcb != NULL)
 {
 IP4_ADDR( &DestIPaddr, DEST_IP_ADDR0, DEST_IP_ADDR1, DEST_IP_ADDR2, DEST_IP_ADDR3 );
 
 /* connect to destination address/port */
 tcp_connect(echoclient_pcb,&DestIPaddr,DEST_PORT,tcp_echoclient_connected);
 }
}

/**
 * @brief Function called when TCP connection established
 * tpcb: pointer on the connection contol block
 * err: when connection correctly established err should be ERR_OK 
 * @retval err_t: returned error 
 */
static err_t tcp_echoclient_connected(void *arg, struct tcp_pcb *tpcb, err_t err)
{
 struct echoclient *es = NULL;
 
 if (err == ERR_OK) 
 {
 /* allocate structure es to maintain tcp connection informations */
 es = (struct echoclient *)mem_malloc(sizeof(struct echoclient));
 
 if (es != NULL)
 {
 es->state = ES_CONNECTED;
 es->pcb = tpcb;
 
 sprintf((char*)data, "sending tcp client message %d", (int)message_count++);
 
 /* allocate pbuf */
 es->p_tx = pbuf_alloc(PBUF_TRANSPORT, strlen((char*)data) , PBUF_POOL);
 
 if (es->p_tx)
 { 
 /* copy data to pbuf */
 pbuf_take(es->p_tx, (char*)data, strlen((char*)data));
 
 /* pass newly allocated es structure as argument to tpcb */
 tcp_arg(tpcb, es);
 
 /* initialize LwIP tcp_recv callback function */ 
 tcp_recv(tpcb, tcp_echoclient_recv);
 
 /* initialize LwIP tcp_sent callback function */
 tcp_sent(tpcb, tcp_echoclient_sent);
 
 /* initialize LwIP tcp_poll callback function */
 tcp_poll(tpcb, tcp_echoclient_poll, 1);
 
 /* send data */
 tcp_echoclient_send(tpcb,es);
 
 return ERR_OK;
 }
 }
 else
 {
 /* close connection */
 tcp_echoclient_connection_close(tpcb, es);
 
 /* return memory allocation error */
 return ERR_MEM; 
 }
 }
 else
 {
 /* close connection */
 tcp_echoclient_connection_close(tpcb, es);
 }
 return err;
}

 

 

 

  My code never enters tcp_echoclient_connected(). I am stuck on this from last few days and very little information is available.

I am not using FreeRTOS.

Can you please tell me what am I doing wrong?

Any help would be appreciated.

This topic has been closed for replies.
Best answer by MGogr.1

So I have solved this issue. I modified my .ioc file; Firstly I enabled FreeRTOS. I also enabled Raw API from Lwip configurations.

I also had to switch to Cube IDE from IAR (don't know for what reason, but the same code is not working in IAR Environment).

3 replies

MS.9
Associate III
September 21, 2024

The ethernetif.c code attached shows a MII interface not the RMII, which the Nucleo has. Its also showing the DP83848_PHY_ADDRESS, but the nucleo has a LAN8742. Try looking in the HAL example/CubeMX code for a better offering.

(The HAL examples have something that is nearly what you are trying to do - that will be a good start point into which to add your stuff)

Also double checked the memory configuration.

Take a look at

"How to create a project for STM32H7 with Ethernet and LwIP stack working" by

 @Adam BERLINGER

 

Cheers

Mark

MGogr.1
MGogr.1Author
Senior
September 23, 2024

Sorry, I have attached wrong file for ethernetif.c. I have updated post with right file.

MGogr.1
MGogr.1AuthorBest answer
Senior
October 5, 2024

So I have solved this issue. I modified my .ioc file; Firstly I enabled FreeRTOS. I also enabled Raw API from Lwip configurations.

I also had to switch to Cube IDE from IAR (don't know for what reason, but the same code is not working in IAR Environment).