cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F767 - HAL_UART_Transmit() is not printing the entire data on the hyperterminal

Sam4
Associate

Hello there,

I have created my own example to print the data on HyperTerminal (putty) following the already given example "UART_Printf" but mine is only printing the first char of the data and then stuck forever. 

 

Here is the clock config code 

Sam4_0-1738947124905.png

and uart config:

Sam4_2-1738947206126.png

 

and what I would like to print:

Sam4_1-1738947174654.png

let me know if you need more info.

 

Thanks,

8 REPLIES 8

Please use the code pasting tool, see icon </>  rather than in-lining screen shots of code

Not sure what "message" is defined at, nor how the pins are configured, etc.

The fragment shown should be workable, perhaps look elsewhere for the actual issue.

Like the MSP code, or where ever you enable the clocks and pins, and peripheral, etc.

Is this a custom board?

Does it work if you just run with the default clock?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
KnarfB
Principal III

sizeof should go to line 110, and strlen to line 111. Where & how is message defined?

hth

KnarfB 

/**
  ******************************************************************************
  * @file    Templates/Src/main.c 
  * @author  MCD Application Team
  * @brief   Main program body
  ******************************************************************************
  * @attention
  *
  * Copyright (c) 2016 STMicroelectronics.
  * All rights reserved.
  *
  * This software is licensed under terms that can be found in the LICENSE file
  * in the root directory of this software component.
  * If no LICENSE file comes with this software, it is provided AS-IS.
  *
  ******************************************************************************
  */

/* Includes ------------------------------------------------------------------*/
#include "main.h"


#ifdef __GNUC__
#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
#endif



ADC_HandleTypeDef	adc_handle;
ADC_ChannelConfTypeDef	adc_channel_conf;
__IO uint16_t adc_val = 0;
__IO float temp_cel = 0.0;

UART_HandleTypeDef uart_handle;


/** @addtogroup STM32F7xx_HAL_Examples
  * @{
  */

/** @addtogroup Templates
  * @{
  */

/* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*/
/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/
/* Private function prototypes -----------------------------------------------*/
static void MPU_Config(void);
static void SystemClock_Config(void);
static void Error_Handler(void);
static void CPU_CACHE_Enable(void);

static void init_adc(void);
static void init_adc_channel(void);
static void init_uart(void);

float read_temperature(ADC_HandleTypeDef *adc_handle);

/* Private functions ---------------------------------------------------------*/

/**
  * @brief  Main program
  * @param  None
  * @retval None
  */
int main(void)
{
  /* This project template calls firstly CPU_CACHE_Enable() in order to enable the CPU Cache.
     This function is provided as template implementation that User may integrate 
     in his application, to enhance the performance in case of use of AXI interface 
     with several masters. */

  /* Configure the MPU attributes */
  MPU_Config();

  /* Enable the CPU Cache */
  CPU_CACHE_Enable();

  /* STM32F7xx HAL library initialization:
       - Configure the Flash ART accelerator on ITCM interface
       - Configure the Systick to generate an interrupt each 1 msec
       - Set NVIC Group Priority to 4
       - Low Level Initialization
     */
  HAL_Init();

  /* Configure the system clock to 216 MHz */
  SystemClock_Config();


  /* Add your application code here */
  init_uart();
  init_adc();
  init_adc_channel();

  //start the conversion process
  if(HAL_ADC_Start_IT(&adc_handle) != HAL_OK)
  {
	  Error_Handler();
  }

  /* Infinite loop */
  uint8_t message[] = "UART!\r\n";

  while (1)
  {
	  //temp_cel = read_temperature(&adc_handle);
	  //snprintf(data, 30, "\n\r temperature: %f\n\r", temp_cel);
	  HAL_UART_Transmit(&uart_handle, message, sizeof(message) - 1, HAL_MAX_DELAY);

  }
}


PUTCHAR_PROTOTYPE
{
	HAL_UART_Transmit(&uart_handle, (uint8_t *)&ch, 1, 0xFFFF);

	return ch;
}
/**
  * @brief  System Clock Configuration
  *         The system Clock is configured as follow : 
  *            System Clock source            = PLL (HSE)
  *            SYSCLK(Hz)                     = 216000000
  *            HCLK(Hz)                       = 216000000
  *            AHB Prescaler                  = 1
  *            APB1 Prescaler                 = 4
  *            APB2 Prescaler                 = 2
  *            HSE Frequency(Hz)              = 8000000
  *            PLL_M                          = 8
  *            PLL_N                          = 432
  *            PLL_P                          = 2
  *            PLL_Q                          = 9
  *            PLL_R                          = 7
  *            VDD(V)                         = 3.3
  *            Main regulator output voltage  = Scale1 mode
  *            Flash Latency(WS)              = 7
  * @param  None
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_ClkInitTypeDef RCC_ClkInitStruct;
  RCC_OscInitTypeDef RCC_OscInitStruct;

  /* Enable HSE Oscillator and activate PLL with HSE as source */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
  RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
  RCC_OscInitStruct.HSIState = RCC_HSI_OFF;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
  RCC_OscInitStruct.PLL.PLLM = 8;
  RCC_OscInitStruct.PLL.PLLN = 432;  
  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
  RCC_OscInitStruct.PLL.PLLQ = 9;
  RCC_OscInitStruct.PLL.PLLR = 7;
  if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    while(1) {};
  }
  
  /* Activate the OverDrive to reach the 216 Mhz Frequency */
  if(HAL_PWREx_EnableOverDrive() != HAL_OK)
  {
    while(1) {};
  }
  

  /* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2
     clocks dividers */
  RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;  
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
  if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7) != HAL_OK)
  {
    while(1) {};
  }
}

/**
  * @brief  This function is executed in case of error occurrence.
  * @param  None
  * @retval None
  */
static void Error_Handler(void)
{
  /* User may add here some code to deal with this error */
  while(1)
  {
  }
}

/**
  * @brief  CPU L1-Cache enable.
  * @param  None
  * @retval None
  */
static void CPU_CACHE_Enable(void)
{
  /* Enable I-Cache */
  SCB_EnableICache();

  /* Enable D-Cache */
  SCB_EnableDCache();
}


/**
  * @brief  Configure the MPU attributes
  * @param  None
  * @retval None
  */
static void MPU_Config(void)
{
  MPU_Region_InitTypeDef MPU_InitStruct;

  /* Disable the MPU */
  HAL_MPU_Disable();

  /* Configure the MPU as Strongly ordered for not defined regions */
  MPU_InitStruct.Enable = MPU_REGION_ENABLE;
  MPU_InitStruct.BaseAddress = 0x00;
  MPU_InitStruct.Size = MPU_REGION_SIZE_4GB;
  MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS;
  MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
  MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
  MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
  MPU_InitStruct.Number = MPU_REGION_NUMBER0;
  MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
  MPU_InitStruct.SubRegionDisable = 0x87;
  MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;

  HAL_MPU_ConfigRegion(&MPU_InitStruct);

  /* Enable the MPU */
  HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}

static void init_adc(void)
{
	adc_handle.Instance = ADCx;
	if(HAL_ADC_DeInit(&adc_handle) != HAL_OK)
	{
		Error_Handler();
	}
	adc_handle.Init.Resolution = ADC_RESOLUTION_12B;
	adc_handle.Init.ContinuousConvMode = ENABLE;
	adc_handle.Init.DiscontinuousConvMode = DISABLE;
	adc_handle.Init.NbrOfDiscConversion = 0;
	adc_handle.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
	adc_handle.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T1_CC1;
	adc_handle.Init.DataAlign = ADC_DATAALIGN_RIGHT;
	adc_handle.Init.NbrOfConversion = 1;
	adc_handle.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV4;
	adc_handle.Init.ScanConvMode = DISABLE;
	adc_handle.Init.DMAContinuousRequests = DISABLE;
	adc_handle.Init.EOCSelection = DISABLE;

	if(HAL_ADC_Init(&adc_handle) != HAL_OK)
	{
		Error_Handler();
	}

}

static void init_adc_channel(void)
{
	adc_channel_conf.Channel = ADC_CHANNEL_TEMPSENSOR;
	adc_channel_conf.Rank = 1;
	adc_channel_conf.SamplingTime = ADC_SAMPLETIME_15CYCLES;
	adc_channel_conf.Offset = 0;

	if(HAL_ADC_ConfigChannel(&adc_handle, &adc_channel_conf) != HAL_OK)
	{
		Error_Handler();
	}
}

float read_temperature(ADC_HandleTypeDef *adc_handle)
{
	adc_val = HAL_ADC_GetValue(adc_handle);

	float Vref = 3.3;
	float Vsense = (adc_val * Vref)/4095.0;
	float V25 = 0.76;
	float avg_slope = 0.0025;

	float temp = ((Vsense - V25)/avg_slope) + 25.0;

	return temp;
}

static void init_uart(void)
{
	uart_handle.Instance = USARTx;

	uart_handle.Init.BaudRate   = 9600;
	uart_handle.Init.WordLength = UART_WORDLENGTH_8B;
	uart_handle.Init.StopBits   = UART_STOPBITS_1;
	uart_handle.Init.Parity     = UART_PARITY_ODD;
	uart_handle.Init.HwFlowCtl  = UART_HWCONTROL_NONE;
	uart_handle.Init.Mode       = UART_MODE_TX_RX;
	uart_handle.Init.OverSampling = UART_OVERSAMPLING_16;

	if(HAL_UART_Init(&uart_handle) != HAL_OK)
	{
		Error_Handler();
	}
}

#ifdef  USE_FULL_ASSERT

/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @param  file: pointer to the source file name
  * @param  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t* file, uint32_t line)
{ 
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */

  /* Infinite loop */
  while (1)
  {
  }
}
#endif

/**
  * @}
  */

/**
  * @}
  */

Hi Tesla,

it is my first question here (so was not familiar with how you guys would like to see the code) but anyways here is the entire main.c. @KnarfB  you can see message[] is defined at line 105

@Tesla DeLorean mpu and clock_config are same as in the "UART_Printf" example code. I following the same same example project.

What I want to is achieve is printing the temperature on the terminal (so basically want to combine ADC temperature sensor and uart print example combined) 

Note: Individual examples works but when I created my empty project (template) I am having the above mention isuse

 

Thanks

KnarfB
Principal III

Check the return value of the HAL function call.

Use the most precise clock (HSE?) at a high clock rate to generate precise timing on the serial line.

Try another cable, terminal prog (TeraTerm) and/or computer.

Step into the HAL code, it is open source and try to find out what's going on.

Check the data on the wires using a cheap logic analyzer or scope.

hth

KnarfB

 

I'm not seeing a reason it should fail yet.

Show MSP code enabling UART and GPIO

Have something in Error_Handler() and HardFault_Handler() so can check it's not dying there.

Check SysTick() is working.

Stop in debugger once it fails, determine where it has stopped or is stuck.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

 

void HAL_UART_MspInit(UART_HandleTypeDef *huart)
{
  GPIO_InitTypeDef  GPIO_InitStruct;

  RCC_PeriphCLKInitTypeDef RCC_PeriphClkInit;

  /*##-1- Enable peripherals and GPIO Clocks #################################*/
  /* Enable GPIO TX/RX clock */
  USARTx_TX_GPIO_CLK_ENABLE();
  USARTx_RX_GPIO_CLK_ENABLE();

  /* Select SysClk as source of USART1 clocks */
  RCC_PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART1;
  RCC_PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_SYSCLK;
  HAL_RCCEx_PeriphCLKConfig(&RCC_PeriphClkInit);

  /* Enable USARTx clock */
  USARTx_CLK_ENABLE();

  /*##-2- Configure peripheral GPIO ##########################################*/
  /* UART TX GPIO pin configuration  */
  GPIO_InitStruct.Pin       = USARTx_TX_PIN;
  GPIO_InitStruct.Mode      = GPIO_MODE_AF_PP;
  GPIO_InitStruct.Pull      = GPIO_PULLUP;
  GPIO_InitStruct.Speed     = GPIO_SPEED_FREQ_VERY_HIGH;
  GPIO_InitStruct.Alternate = USARTx_TX_AF;

  HAL_GPIO_Init(USARTx_TX_GPIO_PORT, &GPIO_InitStruct);

  /* UART RX GPIO pin configuration  */
  GPIO_InitStruct.Pin = USARTx_RX_PIN;
  GPIO_InitStruct.Alternate = USARTx_RX_AF;

  HAL_GPIO_Init(USARTx_RX_GPIO_PORT, &GPIO_InitStruct);
}

/**
  * @brief UART MSP De-Initialization
  *        This function frees the hardware resources used in this example:
  *          - Disable the Peripheral's clock
  *          - Revert GPIO and NVIC configuration to their default state
  * @param huart: UART handle pointer
  * @retval None
  */
void HAL_UART_MspDeInit(UART_HandleTypeDef *huart)
{
  /*##-1- Reset peripherals ##################################################*/
  USARTx_FORCE_RESET();
  USARTx_RELEASE_RESET();

  /*##-2- Disable peripherals and GPIO Clocks #################################*/
  /* Configure UART Tx as alternate function  */
  HAL_GPIO_DeInit(USARTx_TX_GPIO_PORT, USARTx_TX_PIN);
  /* Configure UART Rx as alternate function  */
  HAL_GPIO_DeInit(USARTx_RX_GPIO_PORT, USARTx_RX_PIN);

}

 

@Tesla DeLorean  here is the code for uart msp init

 

sometimes it stuck at:

 tickstart = HAL_GetTick(); 

in HAL_UART_Transmit() function

 

I have found the issue. Issue was with adc initialization, I guess some kind of priority, I need to look into this, but if I comment out the adc() and adc_channel() init function uart works. 

what could have caused it? is it systick interrupt priority vs adc interrupt priority?

/* Add your application code here */
  init_uart();
  //init_adc();
  //init_adc_channel();

  //start the conversion process
  //if(HAL_ADC_Start_IT(&adc_handle) != HAL_OK)
  //{
//	  Error_Handler();
 // }

  /* Infinite loop */
  uint8_t message[] = "UART!\r\n";
  uint8_t data[50];
  uint8_t error = 0;
  float k = 20.50;
  while (1)
  {
	  //temp_cel = read_temperature(&adc_handle);
	  snprintf(data, sizeof(data), "\n\r temperature:%0.2f \n\r", k);
	  HAL_UART_Transmit(&uart_handle, data, sizeof(data), HAL_MAX_DELAY);


  }
}

 

When transmitting a string, use strlen, not sizeof

 

int main() {
    uint8_t data[50];
    float k = 20.50;
    uint32_t _sizeof = 0;
    uint32_t _strlen = 0;

    printf("string to send...");
    snprintf(data, sizeof(data), "\n\r temperature:%0.2f \n\r", k);

    printf("%s", data);
    
    _sizeof = sizeof(data);
    _strlen = strlen(data);
    
    printf("sizeof message: %d\n", _sizeof);
    printf("strlen message: %d\n", _strlen);

    return 0;
}

 

With sizeof, you'll get will always be transmitting 50 elements. With strlen, you'll transmit the correct string length

string to send...

 temperature:20.50 

sizeof message: 50 // incorrect length
strlen message: 23 // correct length

 

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.