2019-04-30 2:03 AM
Hello,
i have a Nucleo-144 board, where i replaced the STM32F429ZI for a STM32F439ZI.
I used CubeMX 5.2.0 to create a ethernet test project just to ping the board and go further from there, but i cant get it to work.
Ethernet is enabled
Ethernet interrupt is enabled.
The parameter settings:
And the advanced parameter settings:
The clock configuration:
LwIP is enabled, general settings (Ive tested with bot static and dynamic IP, both wont work):
I left most of the LwIP options at standart, except i set
LWIP_BROADCAST_PING (Respond to Broadcast Pings) Enabled
LWIP_MULTICAST_PING (Respond to Multicast Pings) Enabled
Also CHECKSUM_BY_HARDWARE is enabled, as well as all the CHEKSUM_GEN_*** and CHECKSUM_CHECK_***
Ive build the source code with Minimum Heap Size 0x2000 and Minimum Stack Size 0x4000.
In Atollic TrueSTUDIO 9.0.1 ive build the project, where i needed to copy fsdata.c to Middlewares/Third_Party/LwIP/src/apps/httpd/ and exclude it from build, so the file would build properly.
I added MX_LWIP_Process(); to the while(1) in main.c, compiled and flashed the board.
At this point i should be able to ping it already, but i get no response whatsoever.
It doesnt matter if i use a crossed or straight ethernet cable, connect it to the network or directly to the PC and if i give a static or dynamic IP, i cant ping the board at all.
Im in a dead end with this, i suspect that the F439ZI MCU on a F429ZI nucleo board wont work, but at this point i dont know what could be wrong. Any tipps/help would be appreciated.
Solved! Go to Solution.
2019-05-01 6:31 AM
Hi
you didn't mention that you called MX_LWIP_Init() before the while loop to initialize LWIP
When use HTTPD , httpd_init(); must be called also.
In LWIP-> "Debug" tab ->advanced options can activate some debug options to help solve the issue.
You can retarget these messages to Atollic's SWV console or to a serial port .
2019-05-01 6:31 AM
Hi
you didn't mention that you called MX_LWIP_Init() before the while loop to initialize LWIP
When use HTTPD , httpd_init(); must be called also.
In LWIP-> "Debug" tab ->advanced options can activate some debug options to help solve the issue.
You can retarget these messages to Atollic's SWV console or to a serial port .
2019-05-03 12:03 AM
Hello and sorry for the late reply.
The MX_LWIP_Init(); is automatically called in the CubeMX generated code:
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_LWIP_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
//Read a received packet from the Ethernet buffers and send it to the LwIP stack for handling
MX_LWIP_Process();
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
Thanks for the hint with the debug options, going to check on that.
EDIT: I deactivated the HTTPD and enabled LWIP_NETIF_LINK_CALLBACK and LWIP_NETIF_REMOVE_CALLBACK, after that the board responds to pings, now i can proceed.
Thanks for the hint with httpd_init();
I searched for that command, but in the whole project i could not find it, so i disabled it in CubeMX.
2019-05-03 5:35 AM
After i enabled LWIP_HTTPD, LWIP_HTTPD_CGI and LWIP_HTTPD_SSI and added httpd_init(); to main.c,i get the compiler error:
"undefined reference to 'httpd_cgi_handler'
in path /EthernetTest/Middlewares/Third_Party/LwIP/src/apps/httpd
The problem: httpd.h, where httpd_cgi_handler is defined, is called with #include "lwip/apps/httpd.h".
The compiler always searches in the wrong place, the httpd.h is located at /EthernetTest/Middlewares/Third_Party/LwIP/src/include/lwip/apps/
but the compiler wont take that path.
The path is given in Properties -> c/c++ Build -> Settings -> Directories -> Include Path
and also in Properties -> C/C++ General -> Paths and Symbols -> Includes
Any idea why the compiler wont take the .h file with the definition of httpd_cgi_handler in the given location?
2019-05-03 10:20 AM
If You have #include "lwip/apps/httpd.h" in file, then configure directory search path to /EthernetTest/Middlewares/Third_Party/LwIP/src/include/ so that concatenated together they form the needed full path.
2019-05-05 11:28 PM
The problem with this is, i already have the search patch .../Middlewares/Third_Party/LwIP/src/include/ enabled, also set it at a higher priority then .../Middlewares/Third_Party/LwIP/src/apps/httpd, but the compiler still gives this error.
I found the source of the problem though: The function httpd_cgi_handler(); is called
httpd_cgi_handler(uri, count, http_cgi_params, http_cgi_param_vals
#if defined(LWIP_HTTPD_FILE_STATE) && LWIP_HTTPD_FILE_STATE
, hs->handle->state
#endif
);
and also declared in the header httpd.h
extern void httpd_cgi_handler(const char* uri, int iNumParams, char **pcParam, char **pcValue
#if defined(LWIP_HTTPD_FILE_STATE) && LWIP_HTTPD_FILE_STATE
, void *connection_state
#endif
);
but there is no function definition. Its simply missing. So i put the function call into comments and the code compiled as it should.
I guess thats a bug with the generated code from CubeMX.
2019-05-06 2:20 AM
Hi.
httpd_cgi_handler(..) must be defined by the user.
In general, when the user wants to install one or more CGI callbacks , must use http_set_cgi_handlers(CGI_arr, x);
CGI_arr is an array of tCGI type, "x" is the number of handlers contained in the array
Install one callback func like this "tCGI CGI_arr[1]={{"/config.cgi", usrCGIHandler}}; //usrCGIHandler is the user handler
So you can call http_set_cgi_handlers(CGI_arr, 1); to install this handler.
2019-05-06 2:54 AM
A "workaround" not to have this link error is to disable
this "HTTP CGI NEW STYLE"
Here are some data from LWIP site
2019-05-06 3:15 AM
Thank you for the great help, i see now where i made my mistakes. Not the answer to the original question, but perfect answer to the followup.
Thanks again.
2020-10-15 12:10 PM
Hello,
How did you solve this issue. I'm having a same problem with httpd_cgi_handler();?
Thank you!