cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407 Flash ERASE/WRITE error only after boot

MRaff.1
Associate III

Hello, 

     on an STM32F407 I am experiencing a Flash Erase/Write error. The odd things is that it happen only the first time after boot, the following times after the error I can write with no errors. 

But, if I erase and write in the Init phase, before the FreeRTOS tasks start, it always work.

The write operation is performed by a state machine called from FREERTOS DefaultTask().

The first state Erase the flash, the second state write a structure stored on RAM. 

I tried to change the size of the writed chunck (FLASH_TYPEPROGRAM_xxx) ant to use the HAL_FLASHEx_Erase() function but the problem persists.

I get the error from the write phase but FLASH_Erase_Sector() does not return a status so I think the error could be in the erase phase.

Any suggestion?

Thank you

 

 

#define FLASH_STORAGE_PAGE_SIZE         0x20000			//128kB
#define FLASH_STORAGE_ADDRESS    		0x080E0000		//Punto all'inizio dell'ultima pagina in flash
#define FLASH_STORAGE_SECTOR 			FLASH_SECTOR_11


HAL_StatusTypeDef flash_erase(void)
{
	HAL_StatusTypeDef res;
	//Instantiate the FLASH_EraseInitTypeDef struct needed for the HAL_FLASHEx_Erase() function
	res = HAL_FLASH_Unlock();
	if (HAL_OK == res)
	{
		FLASH_Erase_Sector(FLASH_SECTOR_11, VOLTAGE_RANGE_3);

		res |= HAL_FLASH_Lock();
	}

	return res;
}


HAL_StatusTypeDef storageSave(void)
{
	uint32_t *pdata;
	int sz = 0;
	HAL_StatusTypeDef res;

	res = flash_erase();

	res |= HAL_FLASH_Unlock();
	pdata = (uint32_t*)&m_ram_param;	
	m_ram_param.size = sizeof(PARAM_t);

	uint32_t crc_val = HAL_CRC_Calculate(&hcrc, (uint32_t*)(&m_ram_param), (sizeof(PARAM_t)-4)/4);

	m_ram_param.flashCRC = crc_val;

	while (sz < sizeof(PARAM_t))
	{
		
		res |= HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, FLASH_STORAGE_ADDRESS + sz, (uint32_t)(*pdata));
		pdata++;		
		sz += 4;		
	}
	res |= HAL_FLASH_Lock();

	return res;
}

 

 

2 REPLIES 2
Andrew Neil
Super User

What error do you get?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
MRaff.1
Associate III

I get an HAL_ERROR from the first call of 

HAL_FLASH_Program()

the calls that follows seems ok but data is not written correclty.

The error comes from FLASH_WaitForLastOperation() an the following flags are set:

Programming parallelism error: FLASH_FLAG_PGPERR

Programming sequence error: HAL_FLASH_ERROR_PGS