2021-10-04 6:49 AM
Hi community..
I have the following code :
bool FLASH_WriteDoubleWord(uint32_t flashAddress, uint64_t Data)
{
FLASH_Unlock();
/*clear some flag*/
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR | FLASH_FLAG_PGSERR );
//FLASH_Erase_Sector(2, 2);
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR | FLASH_FLAG_PGSERR );
/* Program the user Flash area word by word */
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, (uint32_t)&flashAddress, Data) != HAL_OK)
{
FLASH_Lock();
return false;
}
FLASH_Lock();
return true;
}
where
static uint32_t address_test = 0x08008000;
static uint64_t data_test = 0xAAAAAAAA;
I don't understand why the erase part is working instead HAL_FLASH_Program it is not writing the data in the expected address.
Can you please tell me why in your opinion?
Thanks a lot.
Simone
2021-10-04 7:11 AM
Hello @SGasp.1 ,
The reference manual says:
The write access type (byte, half-word, word or double word) must correspond to the type of parallelism chosen (x8, x16, x32 or x64).
If not, the write operation is not performed and a program parallelism error flag (PGPERR) is set in the FLASH_SR register.
So, check if there is an error with the FLASH_SR register prior to calling HAL_FLASHEx_Erase.
Hope my answer helped you! and please keep us informed about your progress on this issue.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
2021-10-04 7:28 AM
FLASH_Erase_Sector is not meant to be called directly. Use HAL_FLASHEx_Erase instead.
2021-10-04 11:39 PM
Hi TDK ... the instruction that is not working it is the following ..
HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, (uint32_t)&flashAddress, Data) != HAL_OK)
2021-10-04 11:46 PM
Don't want the address of parameter variable. Need to pass the address as a uint32_t
2021-10-04 11:52 PM
Can you provide a working example Tesla ?
Thanks a lot .
This is the function that I am calling
* @brief Program byte, halfword, word or double word at a specified address
* @param TypeProgram Indicate the way to program at a specified address.
* This parameter can be a value of @ref FLASH_Type_Program
* @param Address specifies the address to be programmed.
* @param Data specifies the data to be programmed
*
* @retval HAL_StatusTypeDef HAL Status
*/
HAL_StatusTypeDef HAL_FLASH_Program(uint32_t TypeProgram, uint32_t Address, uint64_t Data)
{
HAL_StatusTypeDef status = HAL_ERROR;
/* Process Locked */
__HAL_LOCK(&pFlash);
/* Check the parameters */
assert_param(IS_FLASH_TYPEPROGRAM(TypeProgram));
/* Wait for last operation to be completed */
status = FLASH_WaitForLastOperation((uint32_t)FLASH_TIMEOUT_VALUE);
if(status == HAL_OK)
{
if(TypeProgram == FLASH_TYPEPROGRAM_BYTE)
{
/*Program byte (8-bit) at a specified address.*/
FLASH_Program_Byte(Address, (uint8_t) Data);
}
else if(TypeProgram == FLASH_TYPEPROGRAM_HALFWORD)
{
/*Program halfword (16-bit) at a specified address.*/
FLASH_Program_HalfWord(Address, (uint16_t) Data);
}
else if(TypeProgram == FLASH_TYPEPROGRAM_WORD)
{
/*Program word (32-bit) at a specified address.*/
FLASH_Program_Word(Address, (uint32_t) Data);
}
else
{
/*Program double word (64-bit) at a specified address.*/
FLASH_Program_DoubleWord(Address, Data);
}
/* Wait for last operation to be completed */
status = FLASH_WaitForLastOperation((uint32_t)FLASH_TIMEOUT_VALUE);
/* If the program operation is completed, disable the PG Bit */
FLASH->CR &= (~FLASH_CR_PG);
}
/* Process Unlocked */
__HAL_UNLOCK(&pFlash);
return status;
}
Simone
2021-10-05 12:16 AM
I changed the code in this way ...
uint64_t Data = 1000;
uint32_t address_test = 0x08008090;
FLASH_WriteDoubleWord(address_test , Data);
bool FLASH_WriteDoubleWord(uint32_t flashAddress, uint64_t Data)
{
FLASH_Unlock();
/*clear some flag*/
FLASH_EraseSectors(2, 1); /*working*/
/* Program the user Flash area word by word */
if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, flashAddress, Data) != HAL_OK) /*not working*/
{
FLASH_Lock();
return false;
}
FLASH_Lock();
return true;
}
Nothing to do...
Please help
2021-10-05 12:19 AM
Without the ampersand '&'
2021-10-05 12:22 AM
I tried to remove but nothing to do
2021-10-05 12:51 AM
Well it is surely not the address of the variable. Is the function returning an error? Is the ART still caching it? Print out the address passed, print out the flags status.