cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 UART NOT WORKING CORRECTLY

AlexanderKibarov
Associate III

In the code I have written here, I am trying to send data from UART4 within the main function and simultaneously receive data through interrupts if data arrives. However, the data transmission part works for a very short time and then stops, and the data received from the interrupt is corrupted. I am providing the code from the main.c and stm32f4xx_it.c files below. Can you help me?

main.c:

 

#include "main.h"
#include "kibar_nextion.h"
#include <string.h>

uint8_t main_buffer[5];
uint8_t main_buffer1[8];

int main(void)
{
__HAL_UART_ENABLE_IT(&huart4, UART_IT_RXNE);

uint8_t last_data[] = {255, 255, 255};

while (1)
{
  for(int i = 0; i < 360; i++) {
    HAL_UART_Transmit(&huart4, (uint8_t*)"main_screen.z0.val=", 19, 100);

    HAL_UART_Transmit(&huart4, (uint8_t*)kibar_return_array_char_from_32_t(i), 
      kibar_size_integer_data_32_t(i), 100);

    HAL_UART_Transmit(&huart4, last_data, 3, 100);
  }
}
}

 

stm32f4xx_it.c:

 

#include "main.h"
#include "stm32f4xx_it.h"

extern UART_HandleTypeDef huart4;
extern uint8_t main_buffer[5];
extern uint8_t main_buffer1[8];

void UART4_IRQHandler(void)
{
 HAL_UART_Receive(&huart4, main_buffer, 5, 100);

 HAL_UART_Receive(&huart4, main_buffer1, 8, 100);

 HAL_UART_IRQHandler(&huart4);
}

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

Hello Sir, In a way that I didn't understand, when I put this code:

HAL_UART_Receive_IT(&huart4, main_buffer, 13, 100);

under this code:

HAL_UART_IRQHandler(&huart4);

everything got better. Thank You.

View solution in original post

9 REPLIES 9

Please see the posting tips for how to properly post source code; also, other details needed:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 

You're right. I fixed it. 

And the other things:

  • details of what hardware you're using
  • details of how you're connecting to the UART, providing input, and observing output
  • What testing/debugging/investigation you have done so far
  • etc

Remember, we know nothing about your project other than what you clearly describe in your posts

This is not right!

 

void UART4_IRQHandler(void)
{
   HAL_UART_Receive(&huart4, main_buffer, 5, 100);

   HAL_UART_Receive(&huart4, main_buffer1, 8, 100);

   HAL_UART_IRQHandler(&huart4);
}

 

HAL_UART_Transmit is a blocking receive; ie,  it stops and waits for characters to arrive.

You use this when doing non-interrupt receiving - it's not going to work within the ISR!

HAL_UART_Receive_IT is for interrupt-driven receive.

Please take a look at the HAL documentation, and the examples available in Cube ...


@Andrew Neil wrote:

HAL_UART_Receive_IT is for interrupt-driven receive.

Please take a look at the HAL documentation, and the examples available in Cube ...


As @TDK said in your other thread:

https://community.st.com/t5/stm32-mcus-embedded-software/doesn-t-work-uart-interrupt/td-p/699762

Hello, thank you for your response. I did as you suggested. The code is as follows:

 

void UART4_IRQHandler(void)
{
  /* USER CODE BEGIN UART4_IRQn 0 */
	HAL_UART_Receive_IT(&huart4, main_buffer, 5);
	HAL_UART_Receive_IT(&huart4, main_buffer1, 8);
  /* USER CODE END UART4_IRQn 0 */
  HAL_UART_IRQHandler(&huart4);
  /* USER CODE BEGIN UART4_IRQn 1 */

  /* USER CODE END UART4_IRQn 1 */
}

 

Yes, the interrupt works, but there are some problems. Firstly, I am using the UART connection on the STM32F413ZH board and trying to send and receive data from a Nextion screen. There is no problem when I only send data, and there is no problem when I only receive data. However, when both are done simultaneously, problems start to occur. From the Nextion screen, the first 5 bytes received are a name, followed by an 8-byte number. When I implemented your suggestion, the data transmission part improved, but as shown in the attached image, the 5-byte data is not received correctly, and the 8-byte data is not received at all.

Ekran görüntüsü 2024-07-20 133955.png

Another solution I can think of is to directly read either 13 bytes at once or read one byte at a time and save it into a 13-byte buffer. However, when I do this, I encounter the following result.

Ekran görüntüsü 2024-07-20 134911.png

As you can see, the received data is still corrupted. However, if I turn off data transmission, then the first received data is correct, but data reception will stop. Here's the code where I have disabled data transmission and the image of the received data:

Main.c:

 

#include "main.h"


#include "kibar_nextion.h"

#include <string.h>


uint8_t main_buffer[13];


int main(void)

{
__HAL_UART_ENABLE_IT(&huart4, UART_IT_RXNE);

while (1)

{

}

}

 

 

stm32f4xx_it.c:

 

#include "main.h"

#include "stm32f4xx_it.h"


extern UART_HandleTypeDef huart4;

extern uint8_t main_buffer[13];


void UART4_IRQHandler(void)

{

HAL_UART_Receive_IT(&huart4, main_buffer, 13, 100);

HAL_UART_IRQHandler(&huart4);

}

 

 

Ekran görüntüsü 2024-07-20 135840.png

 

I believe I have explained my issue in more detail this time. Thank you for your help if you can assist me.

You can't queue in this fashion, the functions return immediately, you can only have one operation "in-flight" at a time.

HAL_UART_Receive_IT(&huart4, main_buffer, 5);
HAL_UART_Receive_IT(&huart4, main_buffer1, 8);

You're expected to manage the queuing, or scatter-gather behaviour

You call  HAL_UART_IRQHandler(&huart4); to allow HAL to execute the callbacks, and it's in the callbacks that you manager your buffers and lists, and light-off the next HAL_UART_Receive_IT()

You don't have to embrace the call-back paradigm, but you have to chose one method or another

 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hello Sir, In a way that I didn't understand, when I put this code:

HAL_UART_Receive_IT(&huart4, main_buffer, 13, 100);

under this code:

HAL_UART_IRQHandler(&huart4);

everything got better. Thank You.