2024-08-13 11:58 PM
Hello,
I am using a STM32F427 to read and write data to EEPROM Serial 256-Kb SPI
CAT25256. I use LL API, and DMA full-duplex over SPI. I manage myself the Chip Slect signal.
I can see with logic analyser that datas are sent and received to/from EEPROM correctly.
But I do not have interruption from DMA, neither input or outputstream.
I do not understand why.
The only way to detect the end of the transfer is to look at the BSY flag LL_SPI_IsActiveFlag_BSY(pSPI_Instance). Could-you help me to find where is the problem?
Thank you for help.
Best regards,
FWX.
I