2024-10-07 03:45 AM - last edited on 2024-10-07 04:49 AM by SofLit
Dear Members,
I'm using the STM32F030CC controller for my RTOS-based project and currently developing a bootloader for it. The application code has been relocated to 0x08004000. The bootloader successfully jumps to the application, but after initializing all peripherals (GPIO, timers, etc.), calling `HAL_GetTick()` returns a `uwTick` value of 0.
This is the fuction iam using to jump from bootloader to application. when i try to do _enable_irq(); the jump fuction is not working .
am i missing anything?
2024-10-07 03:47 AM
Please see the Posting Tips for how to properly post source code - not as an image:
2024-10-07 03:48 AM - edited 2024-10-07 03:48 AM
Hello @Sid_sid and welcome to the community,
First, please use </> button to paste your code instead of sharing screen shots.
Second, Did you remap your vector table (VTOR) to the new Flash address 0x08004000?
2024-10-07 04:18 AM
Thankyou for your reply.
are you asking about the linker script in application?
* Specify the memory areas */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 32K
FLASH (rx) : ORIGIN = 0x08004000, LENGTH = 240K
}
2024-10-07 04:38 AM - edited 2024-10-07 04:39 AM
No,
I'm talking about vector table relocation on STM32F0:
2024-10-07 04:57 AM
You are disabling interrupts which prevents systick from occurring.
For working code on how to jump to the bootloader, see here: It can be easily modified to jump instead to your application. Note the section where it disables interrupts in the NVIC registers. You likely need something similar
How to jump to system bootloader from application ... - STMicroelectronics Community
2024-10-07 06:09 AM
actually i mapped vector table to
memcpy((void*)0x20000000, (const void*)APP_ADDRESS, 0xC0);
0x20000000