cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Cube and Azure RTOS hands-on workshop - missing 'STM32-AZURE-RTOS-WS-material.exe' file

Matthew1
Associate II

Hi,

The STM32Cube and Azure RTOS hands-on workshop MOOC is missing the example workshop material file. The MOOC link takes one to a single PDF with setup instructions which include a link for "STM32-AZURE-RTOS-WS-Material.exe". This required file is missing from the Google Drive location.

Could you please make the workshop materials available?

1. MOOC page:

Matthew1_2-1740159599703.png

2. Google Drive link from above MOOC:

Matthew1_3-1740159606704.png

3. Workshop setup PDF with link to materials which takes one back to step (2) above:

Matthew1_4-1740159623138.png

Many thanks,
Matthew.

1 REPLY 1
STTwo-32
ST Employee

Hello @Matthew1

I will check on this with The concerned team after the weekend and I will get back to you ASAP.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.