2021-04-30 3:36 AM
What is new in STM32 USB Host Library v3.4.0?
* Core driver :
* All Classes :
Download link:
https://github.com/STMicroelectronics/stm32_mw_usb_host
Previous Releases information
Details about the content of different USB Host releases are available in the release note:
Overview of the STM32 MW USB Host Library:
https://wiki.st.com/stm32mcu/wiki/USB_overview#USB_host_library_overview
2022-05-03 12:35 PM
Unfortunately, this is still incompatible with any GPLed (2.0 and 3.0) software.
The majority of the ST code is available under BSD-3-Clause, allowing incorporation into any project.
There are plenty of projects which are under an GPL license, but include the ST Middleware, totally unaware any compiled binary is non-distributable.
Whats the reason for this licensing scheme? It will not stop any counterfeit or clone manufacturers, but causes trouble for everyone creating STM32x firmwares.
2022-05-03 2:29 PM
Still no hub support? :(
2022-05-03 3:50 PM
Take a look on TinyUSB. While the host stack development has only started recently, it has an initial hub support. Though I am only using the device stack and cannot comment much about the host part.
And the licence is MIT, so no headaches with that one.