cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 I2C Not Working with Other Interrupts

AlexanderKibarov
Associate III

Hello, I'm using the STM32F413ZH board to read data from the MPU6050. While the data retrieval works when I implement it in a blank project, it fails to function correctly in my current project. This project also includes two additional UART interrupts, though they are not currently connected to the system. What might be causing the issue?

In this project, HAL_StatusTypeDef always returns HAL_BUSY

Thank You.

 

 

#include "main.h"
#include "string.h"

#define MAX_NMEA_PROTOCOL_CHARACTER_LENGTH_ 82

I2C_HandleTypeDef hi2c1;

UART_HandleTypeDef huart4;
UART_HandleTypeDef huart5;
UART_HandleTypeDef huart3;

PCD_HandleTypeDef hpcd_USB_OTG_FS;

void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART3_UART_Init(void);
static void MX_USB_OTG_FS_PCD_Init(void);
static void MX_UART4_Init(void);
static void MX_UART5_Init(void);
static void MX_I2C1_Init(void);

HAL_StatusTypeDef hal_status_one;  //THIS CODE FOR I2C 
uint8_t data_mpu[1] = {0x00};  //THIS CODE FOR I2C 

struct Data_Struct {
	uint8_t leds_mode;
	uint8_t windows_angle;
	uint8_t turn_home;
	uint8_t tilt_protect;
	uint8_t turn_capsize;
} KIBAR_DATA;

uint8_t last_data[3] = { 255, 255, 255 };
uint8_t private_array[1];
uint8_t template_buffer[12] = { 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
		0x00, 0x00, 0x00, 0x00 };
uint8_t instruction_buffer[2] = { 0x00, 0x00 };
uint8_t main_buffer[5] = { 0x00, 0x00, 0x00, 0x00, 0x00 };
volatile uint8_t ff_index = 0;
volatile uint8_t array_index = 0;
volatile uint8_t is_there_back = 0;

volatile uint8_t gps_counter = 0;
volatile uint8_t mode_register = 0;
uint8_t private_gps_buffer[1] = { 0x00 };
uint8_t template_gps_buffer[MAX_NMEA_PROTOCOL_CHARACTER_LENGTH_];
uint8_t latitude_gps_buffer[9];
uint8_t longitude_gps_buffer[10];

//Uart NVIC Interrupt(Uart Global Interrupt) Aktif Edilmeli
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) {
	if (huart == &huart4) {
		HAL_UART_Receive_IT(&huart4, private_array, 1);
		if (private_array[0] == 255) {
			ff_index++;
			if (ff_index == 3) {
				if (array_index == 2) {
					for (int i = 0; i < 2; i++) {
						instruction_buffer[i] = template_buffer[i];
					}
					is_there_back = 1;
				} else if (array_index == 5) {
					for (int i = 0; i < 5; i++) {
						main_buffer[i] = template_buffer[i];
					}
					if (is_there_back == 1) {
						if (instruction_buffer[1] == 108) {
							KIBAR_DATA.leds_mode = main_buffer[1];
						}
						if (instruction_buffer[1] == 119) {
							KIBAR_DATA.windows_angle = main_buffer[1];
						}
						if (instruction_buffer[1] == 104) {
							if (KIBAR_DATA.turn_home == 0)
								KIBAR_DATA.turn_home = 1;
							else
								KIBAR_DATA.turn_home = 0;
						}
						if (instruction_buffer[1] == 116) {
							KIBAR_DATA.tilt_protect = main_buffer[1];
						}
						if (instruction_buffer[1] == 99) {
							if (KIBAR_DATA.turn_capsize == 0)
								KIBAR_DATA.turn_capsize = 1;
							else
								KIBAR_DATA.turn_capsize = 0;
						}
						is_there_back = 0;
					}
				}
				memset(template_buffer, 0x00, 12);
				ff_index = 0;
				array_index = 0;
			}
		} else {
			template_buffer[array_index] = private_array[0];
			array_index++;
		}
	}

	if (huart == &huart5) {
		HAL_UART_Receive_IT(&huart5, private_gps_buffer, 1);
		if (gps_counter == 0 && mode_register == 0
				&& private_gps_buffer[0] == 0x24)
			mode_register = 1;
		if (gps_counter == 0 && mode_register == 0
				&& private_gps_buffer[0] != 0x24)
			mode_register = 2;
		if (mode_register == 1) {
			if (private_gps_buffer[0] == 0x0A) {
				template_gps_buffer[gps_counter] = private_gps_buffer[0];
				if (gps_counter > 30) {
					for (int i = 7; i < 17; i++) {
						if (i != 11) {
							latitude_gps_buffer[i - 7] = template_gps_buffer[i];
						} else continue;
					}
					for (int i = 20; i < 31; i++) {
						if (i != 25) {
							longitude_gps_buffer[i - 20] = template_gps_buffer[i];
						} else continue;
					}
				}
				memset(template_gps_buffer, 0x00, MAX_NMEA_PROTOCOL_CHARACTER_LENGTH_);
				gps_counter = 0;
				mode_register = 0;
			} else {
				template_gps_buffer[gps_counter] = private_gps_buffer[0];
				gps_counter++;
				if (gps_counter == 5) {
					if (!(private_gps_buffer[0] == 0x4C)) {
						memset(template_gps_buffer, 0x00, MAX_NMEA_PROTOCOL_CHARACTER_LENGTH_);
						gps_counter = 0;
						mode_register = 2;
					}
				}
			}
		} else if (mode_register == 2) {
			if (private_gps_buffer[0] == 0x24) {
				template_gps_buffer[gps_counter] = private_gps_buffer[0];
				gps_counter++;
				mode_register = 1;
			}
		}
	}
}

int main(void)
{
  memset(template_gps_buffer, 0x00, MAX_NMEA_PROTOCOL_CHARACTER_LENGTH_);
  memset(latitude_gps_buffer, 0x00, 9);
  memset(longitude_gps_buffer, 0x00, 10);
  KIBAR_DATA.turn_capsize = 0;
  KIBAR_DATA.turn_home = 0;

  HAL_Init();

  SystemClock_Config();

  MX_GPIO_Init();
  MX_USART3_UART_Init();
  MX_USB_OTG_FS_PCD_Init();
  MX_UART4_Init();
  MX_UART5_Init();
  MX_I2C1_Init();

  HAL_UART_Receive_IT(&huart4, private_array, 1);
  HAL_UART_Receive_IT(&huart5, private_gps_buffer, 1);

  while (1) {
    //THIS CODE FOR I2C 
    hal_status_one = HAL_I2C_Mem_Read(&hi2c1, 0xD0, 0x75, 1, data_mpu, 1, 100);
	}
}


static void MX_I2C1_Init(void)
{
  hi2c1.Instance = I2C1;
  hi2c1.Init.ClockSpeed = 100000;
  hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
  hi2c1.Init.OwnAddress1 = 0;
  hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
  hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
  hi2c1.Init.OwnAddress2 = 0;
  hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
  hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
  if (HAL_I2C_Init(&hi2c1) != HAL_OK)
  {
    Error_Handler();
  }
}

static void MX_UART4_Init(void)
{
  huart4.Instance = UART4;
  huart4.Init.BaudRate = 9600;
  huart4.Init.WordLength = UART_WORDLENGTH_8B;
  huart4.Init.StopBits = UART_STOPBITS_1;
  huart4.Init.Parity = UART_PARITY_NONE;
  huart4.Init.Mode = UART_MODE_TX_RX;
  huart4.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart4.Init.OverSampling = UART_OVERSAMPLING_16;
  if (HAL_UART_Init(&huart4) != HAL_OK)
  {
    Error_Handler();
  }
}

static void MX_UART5_Init(void)
{
  huart5.Instance = UART5;
  huart5.Init.BaudRate = 115200;
  huart5.Init.WordLength = UART_WORDLENGTH_8B;
  huart5.Init.StopBits = UART_STOPBITS_1;
  huart5.Init.Parity = UART_PARITY_NONE;
  huart5.Init.Mode = UART_MODE_TX_RX;
  huart5.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart5.Init.OverSampling = UART_OVERSAMPLING_16;
  if (HAL_UART_Init(&huart5) != HAL_OK)
  {
    Error_Handler();
  }
}

static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};

  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOH_CLK_ENABLE();
  __HAL_RCC_GPIOA_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();
  __HAL_RCC_GPIOD_CLK_ENABLE();
  __HAL_RCC_GPIOG_CLK_ENABLE();

  HAL_GPIO_WritePin(GPIOB, LD1_Pin|LD3_Pin|LD2_Pin, GPIO_PIN_RESET);

  HAL_GPIO_WritePin(USB_PowerSwitchOn_GPIO_Port, USB_PowerSwitchOn_Pin, GPIO_PIN_RESET);

  GPIO_InitStruct.Pin = USER_Btn_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  HAL_GPIO_Init(USER_Btn_GPIO_Port, &GPIO_InitStruct);

  GPIO_InitStruct.Pin = LD1_Pin|LD3_Pin|LD2_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

  GPIO_InitStruct.Pin = USB_PowerSwitchOn_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(USB_PowerSwitchOn_GPIO_Port, &GPIO_InitStruct);

  GPIO_InitStruct.Pin = USB_OverCurrent_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  HAL_GPIO_Init(USB_OverCurrent_GPIO_Port, &GPIO_InitStruct);
}

 

 

 

 

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

@AlexanderKibarov wrote:

It was fixed when I switched i2c from 1st to 2nd but i dont know why


You mean you used I2C2 instead of I2C1 ?

Again,  observe what's happening on the I2C lines - what's different ?

As @TDK said, the HAL_BUSY return likely means that one/both line is being held low.

Look at the I2C lines to see if that is, indeed, the case with I2C1 but not I2C2.

If it is the case, then look at the schematic to see why that might be ...

View solution in original post

29 REPLIES 29
Andrew Neil
Evangelist III

@AlexanderKibarov wrote:

it fails to function correctly in my current project.


What does that mean? What, exactly, is failing?

What investigation / testing / debugging have you done to find what's going on? What did you discover?

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 

PS

That's a huuuuuge amount of code within your UART interrupt handler - seldom a good idea!

 

What's going on here:

 

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) {
	if (huart == &huart4) {
		HAL_UART_Receive_IT(&huart4, private_array, 1);
		if (private_array[0] == 255) {
                :
                :

 

You realise that  HAL_UART_Receive_IT returns immediately; it does not wait until your buffer has been filled - or even received anything at all.

 

As i wrote: In this project, HAL_StatusTypeDef always returns HAL_BUSY but when I open an empty project and write the same i2c codes it works fine.


@AlexanderKibarov wrote:

 HAL_StatusTypeDef always returns HAL_BUSY 


As the name suggests, HAL_StatusTypeDef is just a typedef - it cannot "return" anything.

You mean that  HAL_I2C_Mem_Read() returns  HAL_BUSY ?

So try stepping into HAL_I2C_Mem_Read(), and see why it returns  HAL_BUSY 

Also, check the states of your I2C lines - are they valid?

Are you sure you haven't introduced any conflicts when adding the UARTs?

 

See also the PS in my previous post

As I said, the cutting units are not connected anyway, so that part does not work. Actually, even though I tried turning off the uart unit completely, the problem was not solved.

Hello, yes there is no conflict on the uarts. As I mentioned in my previous message, I turned off the uarts completely and it still did not work.

As far as I know, the I2C function returns a value of the HAL_StatusTypeDef types as defined here

typedef enum 
{
  HAL_OK       = 0x00U,
  HAL_ERROR    = 0x01U,
  HAL_BUSY     = 0x02U,
  HAL_TIMEOUT  = 0x03U
} HAL_StatusTypeDef;

 

Andrew Neil
Evangelist III

Not that it should matter, but what's the point of declaring single-element arrays??

uint8_t private_array[1];

 

uint8_t private_gps_buffer[1] = { 0x00 };

:thinking_face:


@AlexanderKibarov wrote:

As far as I know, the I2C function returns a value of the HAL_StatusTypeDef type


That's right the function returns a value - but you said the typedef returns a value.

 


@AlexanderKibarov wrote:

 I turned off the uarts completely and it still did not work.


What does that actually mean?

There could still be conflicts on the GPIOs.

 

Again, have you checked the states of the I2C lines?

 

I would suggest that you proceed as follows:

  1. Go back to your simple project with just the I2C
  2. If that works, then add just one UART, doing a simple, polled echo - no interrupts
  3. If that works, then add the other UART, also doing a simple, polled echo - no interrupts
  4. If that works, then convert just one UART to an interrupt-based echo
  5. If that works, then also convert the other UART to an interrupt-based echo

 

That should identify if there's any fundamental problem, or if the problem lies elsewhere in your original code.

Hello, I removed all the parts related to the uart for you, but I still continue to get HAL_BUSY.

 

#include "main.h"

I2C_HandleTypeDef hi2c1;

void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART3_UART_Init(void);
static void MX_USB_OTG_FS_PCD_Init(void);
static void MX_I2C1_Init(void);

HAL_StatusTypeDef hal_status_one;
uint8_t data_mpu[1] = {0x00};

int main(void)
{
  HAL_Init();

  SystemClock_Config();

  MX_GPIO_Init();
  MX_USART3_UART_Init();
  MX_USB_OTG_FS_PCD_Init();
  MX_I2C1_Init();
	while (1) {
		hal_status_one = HAL_I2C_Mem_Read(&hi2c1, 0xD0, 0x75, 1, data_mpu, 1, 100);
	}
}

void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  __HAL_RCC_PWR_CLK_ENABLE();
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
  RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
  RCC_OscInitStruct.PLL.PLLM = 8;
  RCC_OscInitStruct.PLL.PLLN = 384;
  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
  RCC_OscInitStruct.PLL.PLLQ = 8;
  RCC_OscInitStruct.PLL.PLLR = 2;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
  {
    Error_Handler();
  }
}

static void MX_I2C1_Init(void)
{
  hi2c1.Instance = I2C1;
  hi2c1.Init.ClockSpeed = 100000;
  hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
  hi2c1.Init.OwnAddress1 = 0;
  hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
  hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
  hi2c1.Init.OwnAddress2 = 0;
  hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
  hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
  if (HAL_I2C_Init(&hi2c1) != HAL_OK)
  {
    Error_Handler();
  }
}

static void MX_GPIO_Init(void)
{
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOH_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();
  __HAL_RCC_GPIOD_CLK_ENABLE();
  __HAL_RCC_GPIOG_CLK_ENABLE();
  __HAL_RCC_GPIOA_CLK_ENABLE();

  HAL_GPIO_WritePin(GPIOB, LD1_Pin|LD3_Pin|LD2_Pin, GPIO_PIN_RESET);

  HAL_GPIO_WritePin(USB_PowerSwitchOn_GPIO_Port, USB_PowerSwitchOn_Pin, GPIO_PIN_RESET);

  GPIO_InitStruct.Pin = USER_Btn_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  HAL_GPIO_Init(USER_Btn_GPIO_Port, &GPIO_InitStruct);

  GPIO_InitStruct.Pin = LD1_Pin|LD3_Pin|LD2_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

  GPIO_InitStruct.Pin = USB_PowerSwitchOn_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(USB_PowerSwitchOn_GPIO_Port, &GPIO_InitStruct);

  GPIO_InitStruct.Pin = USB_OverCurrent_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  HAL_GPIO_Init(USB_OverCurrent_GPIO_Port, &GPIO_InitStruct);

}

 


@AlexanderKibarov wrote:

I removed all the parts related to the uart interrupt


But you still have:

  MX_GPIO_Init();
  MX_USART3_UART_Init();
  MX_USB_OTG_FS_PCD_Init();
  MX_I2C1_Init();
  MX_UART4_Init();
  MX_UART5_Init();

That's an awful lot of stuff besides just the I2C !

Again, I would suggest that you proceed as follows:

  1. Go back to your simple project with just the I2C - nothing else
  2. If that works, then add just one UART, doing a simple, polled echo - no interrupts
  3. If that works, then add the other UART, also doing a simple, polled echo - no interrupts
  4. If that works, then convert just one UART to an interrupt-based echo
  5. If that works, then also convert the other UART to an interrupt-based echo

 

That should identify if there's any fundamental problem, or if the problem lies elsewhere in your original code.