cancel
Showing results for 
Search instead for 
Did you mean: 

ST32L476RG dfu bootloader bug via USB?

roland van straten
Associate III
Posted on September 23, 2017 at 15:43

I have a

firmware.dfu

and

firmware.hex

file generated for the

STM32L476RG

. When I use

dfu-util

and upload the file the system doesn't work, if I use my segger jtag interface and uses

SWD

to upload the firmware.hex file everything works as expected. I noticed that some of the code seems to work when using dfu-util, however it looks like a flash sector or so is missing or corrupted.

If it is a problem, is there an

errata

sheet or something about it?

Regards,

Roland

#l476 #dfu
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on September 24, 2017 at 04:37

Pretty sure ST isn't the developer for dfu-util

https://community.st.com/0D50X00009XkeovSAB

https://community.st.com/0D50X00009XkdwKSAR

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

1 REPLY 1
Posted on September 24, 2017 at 04:37

Pretty sure ST isn't the developer for dfu-util

https://community.st.com/0D50X00009XkeovSAB

https://community.st.com/0D50X00009XkdwKSAR

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..