2017-09-23 06:43 AM
I have a
firmware.dfu
andfirmware.hex
file generated for theSTM32L476RG
. When I usedfu-util
and upload the file the system doesn't work, if I use my segger jtag interface and usesSWD
to upload the firmware.hex file everything works as expected. I noticed that some of the code seems to work when using dfu-util, however it looks like a flash sector or so is missing or corrupted.If it is a problem, is there an
errata
sheet or something about it?Regards,
Roland
#l476 #dfuSolved! Go to Solution.
2017-09-23 07:37 PM
Pretty sure ST isn't the developer for dfu-util
https://community.st.com/0D50X00009XkeovSAB
https://community.st.com/0D50X00009XkdwKSAR
2017-09-23 07:37 PM
Pretty sure ST isn't the developer for dfu-util
https://community.st.com/0D50X00009XkeovSAB
https://community.st.com/0D50X00009XkdwKSAR