cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link Utility, Can not connect to target!

zrtn
Associate

zrtn_0-1710845376910.png

16:19:16 : Can not connect to target!
Please select "Connect Under Reset" mode from Target->Settings menu and try again.
If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.
16:19:44 : No target connected

Hi this the error im facing when try to program using stlinkV2 on a custom board

Tried switching to powerdown mode also and also checked the connections of pcb 

 what could be the issue

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

First, ST-Link Utility tool is obsolete so please use STM32CubeProgrammer instead.

Second, check the power supply of your MCU.

Third: are you using one of low power modes in the program already loaded in the MCU?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
SofLit
ST Employee

Hello,

First, ST-Link Utility tool is obsolete so please use STM32CubeProgrammer instead.

Second, check the power supply of your MCU.

Third: are you using one of low power modes in the program already loaded in the MCU?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.