2021-10-27 4:20 AM
Hi
I have a problem where my NUCLEO-U575ZI-Q board gets a hard fault if I use sprintf.
I reproduced the error by creating a new project based on the sample project "Tx_Thread_Sync". So I am using Threadx.
I then added two lines to the app_threadx.c
char str[80];
sprintf(str, "Value of Pi = %u", 3);
And then places a breakpoint at the variable definition. I run the code and when I click on step into the function for debugging the sprintf function the MCU goes directly to HardFault_Handler instead.
Please help.
What to do so I can use sprintf??
Best Regards
Anders
Solved! Go to Solution.
2021-10-29 2:26 AM
Hello @APede.1
The issue is related to the thread stack size.
In the tx_Thread_Sync example, the thread stack size is set to 512B
The thread creation call uses the define APP_STACK_SIZE
Also, the stack is allocated in the byte pool provided as argument of App_ThreadX_Init function.
So, byte pool size needs to be increased accordingly.
To do this, you open the ioc file to get CubeMX interface, go to middlewares/ThreadX and ThreadX Tab. Memory configuration Topic: change ThreadX memory pool size to say 10*1024 to give room for further allocations and re-generated code with CTRL-S or ALT-K
Then in App_ThreadX_Init:
Replace APP_STACK_SIZE by APP_STACK_SIZE*4
if (tx_byte_allocate(byte_pool, (VOID **) &pointer, APP_STACK_SIZE*4, TX_NO_WAIT) != TX_SUCCESS)
And same for thread create:
if (tx_thread_create(&ThreadOne, "Thread One", ThreadOne_Entry, 0, pointer, APP_STACK_SIZE*4, THREAD_ONE_PRIO,
THREAD_ONE_PREEMPTION_THRESHOLD, DEFAULT_TIME_SLICE, TX_AUTO_START) != TX_SUCCESS)
After executing in debug mode you can open the Window/Showview/ThreadX/ThreaXThreadList
In the ThreadX Thread List window, you will need to click on the top left icon with the 3 horizontal lines.
This will activate the Stack Usage column of this view.
On my side I could see a stack usage of 676 bytes when adding this sprintf.
So, you could have increased size to only APP_STACK_SIZE*2 but when you are not sure it is always better to have margin.
Best regards
Jocelyn
2021-10-27 6:45 AM
sprintf can use the heap and may be failing an allocation.
2021-10-27 7:12 AM
I use the standard settings:
_Min_Heap_Size = 0x200 ; /* required amount of heap */
0x200 = 512 bytes
I just tried with
_Min_Heap_Size = 0x2000 ; /* required amount of heap */
0x200 = 8192bytes
Same error - Hard Fault
2021-10-27 10:47 AM
Yeah, so you might have to debug what's actually causing the fault. The processor has a number registers to convey details of the fault, and the context is pushed on the stack.
If you can pin-point the instructions, and addresses it is objecting too you can work toward where the problem is.
Watch stack allocations, perhaps make str[] a static allocation an see if it moves/changes the problems.
Check also what libraries you're linking, the Cortex-M isn't going to run 32-bit ARM code..
2021-10-27 11:29 PM
If define str[] static and then it works.
I then tried to define it in the function and increase the stack size to 0x4000 and 0x40000. But it still fails. Default is 0x400.
When I get hard fault the CFSR register is 0x100000 which seems to be an Unaligned access flag.
Unaligned access flag. Sticky flag indicating whether an unaligned access error has occurred.
Any help/experience in how to avoid that ?
2021-10-29 2:26 AM
Hello @APede.1
The issue is related to the thread stack size.
In the tx_Thread_Sync example, the thread stack size is set to 512B
The thread creation call uses the define APP_STACK_SIZE
Also, the stack is allocated in the byte pool provided as argument of App_ThreadX_Init function.
So, byte pool size needs to be increased accordingly.
To do this, you open the ioc file to get CubeMX interface, go to middlewares/ThreadX and ThreadX Tab. Memory configuration Topic: change ThreadX memory pool size to say 10*1024 to give room for further allocations and re-generated code with CTRL-S or ALT-K
Then in App_ThreadX_Init:
Replace APP_STACK_SIZE by APP_STACK_SIZE*4
if (tx_byte_allocate(byte_pool, (VOID **) &pointer, APP_STACK_SIZE*4, TX_NO_WAIT) != TX_SUCCESS)
And same for thread create:
if (tx_thread_create(&ThreadOne, "Thread One", ThreadOne_Entry, 0, pointer, APP_STACK_SIZE*4, THREAD_ONE_PRIO,
THREAD_ONE_PREEMPTION_THRESHOLD, DEFAULT_TIME_SLICE, TX_AUTO_START) != TX_SUCCESS)
After executing in debug mode you can open the Window/Showview/ThreadX/ThreaXThreadList
In the ThreadX Thread List window, you will need to click on the top left icon with the 3 horizontal lines.
This will activate the Stack Usage column of this view.
On my side I could see a stack usage of 676 bytes when adding this sprintf.
So, you could have increased size to only APP_STACK_SIZE*2 but when you are not sure it is always better to have margin.
Best regards
Jocelyn
2021-10-29 6:34 AM
Hi Jocelyn
I tested it out and it works.
Thank you for your fast help.
Best regards
Anders
2022-11-16 9:25 PM
Thanks RICARD! I was having a similar Hard Fault while in a thread and stack size was the issue. Nicely done!