Source to READ/WRITE txt files from usb
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-10-14 4:49 AM
Hello community!
In the project I'm working on, after the UART communication, I need to configure the USB to be able to read a txt file, creat or write another txt file and to update the frimware.
I'm asking you if there is any source that shows how to do this kind of things. If not, I would like to start reading the txt file in the usb.
I'm using HAL library, FATFS and USB_HOST only with MSC
Thanks for your help!
Solved! Go to Solution.
- Labels:
-
UART-USART
-
USB
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-15 11:15 AM
OP wants a HOST
STM32Cube_FW_F4_V1.25.0\Projects\STM32F4-Discovery\Applications\FatFs\FatFs_USBDisk
STM32Cube_FW_F4_V1.25.0\Projects\STM324x9I_EVAL\Applications\USB_Host\FWupgrade_Standalone
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
2021-11-15 7:27 AM
Hello @OBorr.1 ,
We provide some examples in our Firmware package. You can refer to one of them.
For example, in the F7 CubeFW you can refer to this application:
- Path: Projects\STM32756G_EVAL\Applications\USB_Device\MSC_Standalone.
BeST Regards,
Walid
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-15 11:15 AM
OP wants a HOST
STM32Cube_FW_F4_V1.25.0\Projects\STM32F4-Discovery\Applications\FatFs\FatFs_USBDisk
STM32Cube_FW_F4_V1.25.0\Projects\STM324x9I_EVAL\Applications\USB_Host\FWupgrade_Standalone
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
2021-11-16 12:25 AM
Yes, that's right thank you.
@OBorr.1 you can refer to the examples proposed by @Community member.