cancel
Showing results for 
Search instead for 
Did you mean: 

Error in Release Mode Build: "unterminated variable reference" in subdir.mk

meghasb
Senior

Hi all,

I'm facing an issue while building my STM32 project in Release mode, but everything compiles fine in Debug mode.

The following error appears during the Release build:
Middlewares/usbx/UX_Network_Driver/subdir.mk:19: *** unterminated variable reference. Stop.
make: *** [makefile:85: all] Error 2

There are no issues in any of the other source or header files. This only occurs in the subdir.mk under the USBX network driver middleware.

I would like to understand:

  • What could be the root cause of this error?

  • Why it occurs only in Release mode and not in Debug mode?

  • What steps can I take to resolve this?

Any guidance or suggestions would be greatly appreciated.

Thanks in advance!

1 REPLY 1
Saket_Om
ST Employee

Hello @meghasb 

Did you clean before re-build in release mode?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om