cancel
Showing results for 
Search instead for 
Did you mean: 

So are there successful implementation of

AMish.5
Associate

I'm using STM32F767ZI MCU based Nucleo -F767ZI development board, which is supporting Ethernet communication protocol and so on. I have a motor driver which is supporting the EtherCAT communication interface, and I want to interface that motor driver with Nucleo board using EtherCAT communication method. I have LWIP supported library with Nucleo - F767ZI development board.

Is this communication set up valid for communicating two boards one as master and other as a slave.

Please suggest any solution regarding this.

0 REPLIES 0