2025-04-16 8:02 PM
I am using the DMA in a few places. I am wondering should these variables be volatile. As it is, the compiler has no idea when the data will be read from or written into these variables. When that is the case, shouldn't you make the variable volatile? I don't think I have seen them as volatile in the example code however. Am I missing something here?
2025-04-17 5:56 AM
If using cache, buffers from DMA should be cleaned before writing and invalidated before reading. Volatile here doesn't help.
Buffers should be marked volatile if the value is changing within a function and the function needs the updated value. For example, if you set a flag in an interrupt which you then check for and process in the main flag. (This is a little more complicated since link time optimization can cause functions to become combined, so to speak.)
2025-04-17 6:56 AM - edited 2025-04-17 7:23 AM
If a buffer is initialised (which is always the case for C, if it's not an automatic), then the optimizer can make assumptions about the value it holds. If that buffer is used to hold (say) an SPI command sequence and it is also used to received a response (replacing the original content), then the optimizer may assume that the value has not changed if the receive transfer takes place via DMA:
void f1( void )
{
uint8_t buffer = 0xa5; // Command value
spiDMASendReceive( &buffer );
switch ( buffer )
{
case 0x00: action00(); break; // Eliminated by optimization
case 0x01: action01(); break; // Eliminated by optimization
default: // Only feasible value without 'volatile'
}
}You can see the effect here, where no code is generated for f1(), but it is for f2() as 'volatile' qualification is added.
And yes, caching (hardware) and optimization (compile time) are not the same, but both can appear to "break" the code.
Edited to make it clear that I was referring to hardware caching, not run time caching of calculated values.
2025-04-17 7:02 AM - edited 2025-04-17 7:02 AM
@CTapp.1 wrote:And yes, caching (runtime) and optimization (compile time) are not the same
But the optimisation might be to use "caching" (unlikely in the case of a buffer, but quite possible for a simple int, say).
See the PS to my previous post.
2025-04-17 7:22 AM
That's where we get into terminology and definitions! I was only considering hardware, so will update my reply to reflect that ;)
The language standard doesn't help either, as it does mention "caching" (generally to mean a computed value may be stored in a static buffer* so that the result can be reused), but has nothing to say about optimization other than that it is irrelevant (but the program must behave the same).
* this is generally "design time" optimization made during compiler implementation, where as the elimination of a read would be made during compilation.
2025-04-17 8:41 AM
> Instead of actually reading from memory each time, the compiler might optimise by reading once into a register, and using that.
IIRC this is called register allocation or register optimization. Not caching.