cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103C6T6 CAN bootloder active

Abdul-khalil
Associate II

CAN bootloader for STM32F103C6T6A with an application 

 

  • 1st Stage: Bootloader (loaded via ST-Link/V2)

  • 2nd Stage: Application code (uploaded via CAN)

& How to Let the Application Know Firmware Was Uploaded via CAN

 

1 REPLY 1
mƎALLEm
ST Employee

Hello @Abdul-khalil and welcome to the ST Community,

A question: why the application should know if the application was uploaded over CAN if it is the only interface to update your application? maybe you need to describe your use case?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.