2025-04-13 11:22 AM - last edited on 2025-04-16 7:42 AM by Amel NASRI
Is there any update on this issue? I have similar problem with being not able to initialize SD Card using SDMMC1 + FileX + ThreadX. Getting SDMMC_FLAG_CTIMEOUT while initialization (SD_PowerON() function). Does someone have maybe a working example of using SD Card with FileX on U545 uC?
2025-04-16 7:19 AM - edited 2025-04-16 7:44 AM
Hi @MDaniol ,
I'm moving your post to a new thread as the old one (STM32U545 Nucleo Fails to Initialize SDMMC) was managed directly with the customer via a dedicated support channel (OLS).
You may start with this article and adapt it on your case: How to use FileX with eMMC for file system management.
That would be nice if @aroby95 can come back to provide some help here.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.