2022-06-29 10:50 PM
Dear all,
Now I would like to use TLS on BLE connection because my module cannot use pairing.
So, I was starting to learn about STSAFE-A110, and have bought B-L4S5I-IOT01A. I found X-CUBE-IOTA1 project,and I had mimicked it on CubeMX/IDE bare environment of the development kit instead of import it. And I called stsafe_wrap_unwrap().
As the result, It failed StSafeA_PutAttribute() once as STSAFEA_COMMUNICATION_ERROR. Then, the calling result is always STSAFEA_UNSATISFIED_ACCESS_CONDITION.
Also I called StSafeA_GenerateLocalEnvelopeKey() without PutAttribute, but it also fails as UNSATISFIED.
I also imported the X-CUBE-IOTA1, and execute "STSAFE Wrap/Unwrap". The result is same. pairing_stsafe() falls in UNSATISFIED.
What "UNSATISFIED" means in this case? How can I recover it to "SATISFIED" state?
I found a FAQ page in STCommunity which says the "Host Key" is onetime writable. "A temporary(dummy) key was written and can't change" is acceptable at the development kit, but at least, I would like to use wrap/unwrap function... How should I do?
Best regards,
2022-07-07 1:36 AM
@Benjamin BARATTE @Jocelyn RICARD
Excuse me, dear ST members, could you give me any advice?
Best regards,
2022-07-07 6:36 AM
Hi Takim,
I have check the code and I see that the stsafe_l2sec_init() function always call the stsafe_pairing() which execute the StSafeA_PutAttribute() on the host key slot. This operation is a one-time operation so the first time the return shall be 0x00 and all other time the return will be 0x11 STSAFEA_UNSATIFIED_ACCESS_CONDITION meaning that the Host keys are already set.
As the new call stsafe_PSK_init() return is ORed with the stsafe_pairing() the stsafe_l2sec_init() will always return STSAFEA_UNSATISFIED_ACCESS_CONDITION.
now in the stsafe_wrap_unwrap() function there is a call to the stsafe_pairing() which still return STSAFEA_UNSATISFIED_ACCESS_CONDITION as explained before, then the stsafe_wrap_unwrap() will not work.
What I would recommend is to change the stsafe_pairing() with the following code :
/* Perform pairing between Host MCU and STSAFE (set Host Keys)
* Send host cipher key & host MAC key to STSAFE for pairing
*/
static int stsafe_pairing(void)
{
int status_code = STSAFEA_INVALID_PARAMETER;
uint8_t K_CMAC_Host[32] = {
0x11, 0x11, 0x22, 0x22, 0x33, 0x33, 0x44, 0x44, 0x55, 0x55, 0x66, 0x66, 0x77, 0x77, 0x88, 0x88,
0x00, 0x11, 0x22, 0x33, 0x44, 0x55, 0x66, 0x77, 0x88, 0x99, 0xAA, 0xBB, 0xCC, 0xDD, 0xEE, 0xFF};
StSafeA_HostKeySlotBuffer_t out;
/* check pairing keys */
status_code = StSafeA_HostKeySlotQuery(stsafea_handle, &out, STSAFEA_MAC_NONE);
if (status_code == STSAFEA_OK)
{
if (out.HostKeyPresenceFlag == 0)
{
printf("\nstsafe pairing not set");
status_code = StSafeA_PutAttribute(&stsafea_handle, // STSAFE obj ptr
STSAFEA_TAG_HOST_KEY_SLOT, // Attribute tag
K_CMAC_Host, // dataIn (Keys)
sizeof(K_CMAC_Host), // dataInLen
STSAFEA_MAC_NONE); // MAC
printf("\npairing_stsafe result (0 means success): %d\n", (int)status_code);
}
}
return status_code;
}
in that case, we check if the pairing is already done and if yes, we return STSAFEA_OK.
hope this will help.
Best Regards,
Benjamin
2022-07-08 12:15 AM
Dear @Benjamin BARATTE ,
Thank you for your advice. I have applied your code.
StSafeA_HostKeySlotQuery returns STSAFEA_OK, and the HostKeyPresenceFlag is 1.
But unfortunately, the problem was not improved.
The error is same as previously, as shown as;
>stsafe_wrap_unwrap result (StSafeA_GenerateLocalEnvelopeKey - 0 means success): 17
I have no idea why StSafeA_GenerateLocalEnvelopeKey() returns UNSATISFIED...
Do you have any other advice for this problem?
Further, StSafeA_GenerateLocalEnvelopeKey returns error, but StSafeA_Echo, StSafeA_ProductDataQuery, StSafeA_LifeCycleStateQuery, StSafeA_HostKeySlotQuery, and StSafeA_GenerateRandom are working correctly.
Just in case, I attached the result of LifeCycleStateQuery, and HostKeySlotQuery;
[LifeCycleStateQuery]
Length:1
LifeCycleStatus:3
[HostKeySlotQuery]
Length:4
HostKeyPresenceFlag:1
HostCMacSequenceCounter:1
Best regards,
2022-07-08 12:53 AM
Hi @Takim.l
I forget the generation of the LocalEnvelopKey...
if the local envelop key is already generated, you will get the error 0x11 STSAFEA_UNSATISFIED_ACCESS_CONDITION.
here is code snippet to patch the stsafe_wrap_unwrap() test function to avoid generating the key if already present :
it's for the file stsafe.c around line 481 :
StSafeA_LocalEnvelopeKeyTableBuffer_t out_env;
StSafeA_LocalEnvelopeKeyInformationRecordBuffer_t out_rec0;
StSafeA_LocalEnvelopeKeyInformationRecordBuffer_t out_rec1;
status_code = StSafeA_LocalEnvelopeKeySlotQuery(stsafea_handle, &out_env, &out_rec0, &out_rec1, STSAFEA_MAC_NONE);
if (status_code == STSAFEA_OK)
{
if (out_rec0.PresenceFlag == 0)
{
status_code = StSafeA_GenerateLocalEnvelopeKey(&stsafea_handle,
STSAFEA_KEY_SLOT_0,
STSAFEA_KEY_TYPE_AES_128,
NULL,
0U,
STSAFEA_MAC_NONE);
printf("\n\rstsafe_wrap_unwrap result (StSafeA_GenerateLocalEnvelopeKey - 0 means success): %d\n", status_code);
if(status_code != STSAFEA_OK)
{
return status_code;
}
}
}
printf("\n\rstsafe check envelop key result (StSafeA_LocalEnvelopeKeySlotQuery - 0 means success): %d\n", status_code);
if(status_code != STSAFEA_OK)
{
return status_code;
}
This should unlock the test.
Nevertheless, the L2SEC-PSK implementation using STSAFE-A wrap mechanism should be working on your board as all preliminary step has been fulfilled.
Best Regards,
Benjamin