cancel
Showing results for 
Search instead for 
Did you mean: 

Re: HardFault UDP Client

eduardo_reis
Senior

Split from: https://community.st.com/t5/stm32-mcus-embedded-software/hardfault-udp-client/m-p/716640


I have the same problem. @LEAMtw, I hope you don't mind if I add details here for my scenarios.

Error

 

Thread #1 [main] 1 [core: 0] (Suspended : Signal : SIGTRAP:Trace/breakpoint trap) MemManage_Handler() at stm32h7xx_it.c:105 0x8016138 <signal handler called>() at 0xffffffe9 ethernet_input() at ethernet.c:113 0x802e6c4 ethernetif_input() at ethernetif.c:347 0x8023e18 MX_LWIP_Process() at lwip.c:156 0x8023b6a Firmware::MainRuntimeLoop() at firmware.cc:101 0x80034de Boilerplate_Loop() at boilerplate.cc:16 0x80011d6 main() at main.c:131 0x8015458

 

When debugging, I noticed that `p` buffer is valid, however, the payload is invalid.

eduardo_reis_5-1734044383054.png

 

Name : p Details:0x30004140 <memp_memory_RX_POOL_base+15680> Default:0x30004140 <memp_memory_RX_POOL_base+15680> Decimal:805323072 Hex:0x30004140 Binary:110000000000000100000101000000 Octal:06000040500

 

 

 

Name : payload Details:0x9a000000 Default:0x9a000000 Decimal:-1711276032 Hex:0x9a000000 Binary:10011010000000000000000000000000 Octal:023200000000

 

 

In my case I am not using FreeRTOS, I am using a bare-metal approach instead.

Configuration

I have a STM32H723ZG. This is how things are configured.

## MPU

eduardo_reis_0-1734043881079.png

eduardo_reis_1-1734043914715.png

ETH

eduardo_reis_2-1734043961831.png

LWIP

eduardo_reis_3-1734044012891.png

STM32H723ZGTX_FLASH.ld

eduardo_reis_4-1734044258870.png

 

 

7 REPLIES 7

@eduardo_reis wrote:

 

I have the same problem. @LEAMtw, I hope you don't mind if I add details here for my scenarios.


It may be similar symptoms, but not necessarily the same problem. So best to have your own thread - then you can mark your own solution when done.

 


@eduardo_reis wrote:

In my case I am not using FreeRTOS, I am using a bare-metal approach instead.


Could be quite a significant difference!

Have you tried the previous suggestions:

 


@eduardo_reis wrote:

When debugging, I noticed that `p` buffer is valid, however, the payload is invalid.


Are you passing auto data, so that the data is no longer valid by the time LwIP tries to access it? 

eduardo_reis
Senior

Duplicate - merged.


I have the same problem. @LEAMtw, I hope you don't mind if I add details here for my scenarios.

Error

Thread #1 [main] 1 [core: 0] (Suspended : Signal : SIGTRAP:Trace/breakpoint trap)	
	MemManage_Handler() at stm32h7xx_it.c:105 0x8016138	
	<signal handler called>() at 0xffffffe9	
	ethernet_input() at ethernet.c:113 0x802e6c4	
	ethernetif_input() at ethernetif.c:347 0x8023e18	
	MX_LWIP_Process() at lwip.c:156 0x8023b6a	
	Firmware::MainRuntimeLoop() at firmware.cc:101 0x80034de	
	Boilerplate_Loop() at boilerplate.cc:16 0x80011d6	
	main() at main.c:131 0x8015458	

When debugging, I noticed that `p` buffer is valid, however, the payload is invalid.

eduardo_reis_0-1734097639775.png

Name : p
	Details:0x30004140 <memp_memory_RX_POOL_base+15680>
	Default:0x30004140 <memp_memory_RX_POOL_base+15680>
	Decimal:805323072
	Hex:0x30004140
	Binary:110000000000000100000101000000
	Octal:06000040500

 

Name : payload
	Details:0x9a000000
	Default:0x9a000000
	Decimal:-1711276032
	Hex:0x9a000000
	Binary:10011010000000000000000000000000
	Octal:023200000000

In my case I am not using FreeRTOS, I am using a bare-metal approach instead.

Configuration

I have a STM32H723ZG. This is how things are configured.

MPU

eduardo_reis_1-1734097639852.png

 

eduardo_reis_2-1734097639892.png

 

ETH

eduardo_reis_3-1734097639933.png

 

LWIP

eduardo_reis_4-1734097639929.png

 

STM32H723ZGTX_FLASH.ld

eduardo_reis_5-1734097639924.png

 

 


@eduardo_reis wrote:

 

I have the same problem.

:

When debugging, I noticed that `p` buffer is valid,


That's a different problem: In @LEAMtw's case, the pointer was  invalid, and accessing the invalid memory caused a Hard Fault.

Also, that case was using FreeRTOS - which you're not.

eduardo_reis
Senior

@Andrew Neil thank you for creating the spilt. I ended up duplicating my post cause I didn't get the notification about it and I though my original response didn't go through when note seeing it here. Make more sense to put it as its own thing indeed.

  • Increase stack size
  • Enable diagnostics

By stack size you mean LWIP MEM_SIZE? What should I estimate when defining the stack size?I have it as 14 KB, which to seems to be way above my needs.

I enabled the following debug flags:

 

/*----- Default Value for ETHARP_DEBUG: LWIP_DBG_OFF ---*/ #define ETHARP_DEBUG LWIP_DBG_ON /*----- Default Value for NETIF_DEBUG: LWIP_DBG_OFF ---*/ #define NETIF_DEBUG LWIP_DBG_ON /*----- Default Value for PBUF_DEBUG: LWIP_DBG_OFF ---*/ #define PBUF_DEBUG LWIP_DBG_ON /*----- Default Value for RAW_DEBUG: LWIP_DBG_OFF ---*/ #define RAW_DEBUG LWIP_DBG_ON /*----- Default Value for MEM_DEBUG: LWIP_DBG_OFF ---*/ #define MEM_DEBUG LWIP_DBG_ON /*----- Default Value for MEMP_DEBUG: LWIP_DBG_OFF ---*/ #define MEMP_DEBUG LWIP_DBG_ON /*----- Default Value for UDP_DEBUG: LWIP_DBG_OFF ---*/ #define UDP_DEBUG LWIP_DBG_ON

 

and got the following output on the serial monitor when initialising my application.

 

 

10:38:53.370 -> Assertion "udp_remove: invalid pcb" failed at line 1185 in ../Middlewares/Third_Party/LwIP/src/core/udp.c

Despite the Assertion above, the application was initialised and it seems to be running fine. I have to bring to start publishing udp packages with a certain size in order to make it crash after sometime.

 

I don't see any new message when it crashes.

eduardo_reis
Senior

GPT gave me a lead on a few other things to investigate, and one of them seems to have fixed this issue.

I had a concurrency problem. In my main loop, I had `MX_LWIP_Process`; in another interruption, the LWIP was sending packages. At some point, the interruption would interrupt the `MX_LWIP_Process,` and things would be messed up from then on.

 

Instead of dealing with synchronization, such as semaphores, etc, I simply moved the `MX_LWIP_Process` to the beginning of the interruption, which has worked well so far in my application.

 

I am still getting this assertion failed on the LwIP debug.

 

10:38:53.370 -> Assertion "udp_remove: invalid pcb" failed at line 1185 in ../Middlewares/Third_Party/LwIP/src/core/udp.c

 

 

I still don't understand why, given that my assumption about this being a concurrency problem is correct, the issue did not happen all the time but only in some use cases.

 

In any case, I am marking this as solved. Thank you so much to everyone.

PS: I am un-marking this as the solution because I found the problem is persistent in another test case. So, it turned out this solution is only partial.


@eduardo_reis wrote:

 I simply moved the `MX_LWIP_Process` to the beginning of the interruptio


You mean you're running your entire LwIP Process from an ISR?

That really doesn't sound like a great idea!

eduardo_reis
Senior

@Andrew NeilWhy not? In my case, there is nothing going on in the main loop, and this interrupt has a lower priority than the remaining ones. So, it would still be interrupted by other critical things.

 

Eventually, I want to move to using queues and FreeRTOS, but for now, this is what I have. FreeRTOS has a limitation (from what I understood) of 1000Hz max. I want the UDP packages to be sent faster than that.