cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with SD Card with STM32H743ZIT6

rubenles
Senior

Hello, i am trying to make a file with a text on a SD card without success.

I followed this tutorial:

https://community.st.com/t5/stm32-mcus/how-to-create-a-file-system-on-a-sd-card-using-stm32cubeide/ta-p/49830

But i have a stm32h743zit6 and it is a bit different.First, I can't configure DMA on SDMMC in stm32cubemx.

I've configured the pins of the stm to the pins slot i have in my board (Is a custom board made by me using this microcontroller and the sd card slot.)

I activated in cubemx: DMA (I think it is not necessary), SDMMC, FATFS, GPIO and freertos (for threads in the future).

Then, i wrote a simple code shown in the tutorial:

/* USER CODE BEGIN 1 */ FRESULT res; //Fatfs function common result code uint32_t byteswritten, bytesread; // File writes/read counts uint8_t wtext[]= "PRUEBA ESCRITURA"; //Buffer de escritura de archivo uint8_t rtext[_MAX_SS]; //Lectura de buffer de fichero /* USER CODE END 1 */
/* USER CODE BEGIN 2 */ if(f_mount(&SDFatFS, (TCHAR const*)SDPath, 0) != FR_OK) { printf("Error mount\r\n"); } else { printf("mount correct \r\n"); if(f_mkfs((TCHAR const*)SDPath, FM_ANY, 0, rtext, sizeof(rtext)) != FR_OK) { printf("Error make file\r\n"); } else { printf("File created \r\n"); //Open file for writing (Create) if(f_open(&SDFile, "Prueba_para_ficheros.TXT", FA_CREATE_ALWAYS | FA_WRITE) != FR_OK) { printf("Error writing\r\n"); } else { printf("File opened \r\n"); //Write to the text file res = f_write(&SDFile, wtext, strlen((char *)wtext), (void *)&byteswritten); printf("Writing in file\r\n"); if((byteswritten == 0) || (res != FR_OK)) { } else { printf("File closed\r\n"); f_close(&SDFile); } } } } f_mount(&SDFatFS, (TCHAR const*)NULL, 0); /* USER CODE END 2 */
View more

 

I have an error doing f_mkfs, and the program does not do the opening or writing thing.

rubenles_0-1705580530944.png

 

Can anyone tell me what it could be happening here? Any ideas?

 

Thank you so much!

1 REPLY 1
Saket_Om
ST Employee

Hello @rubenles

You can refer to this application provided in the STM32CubeH7 firmware. It demonstrates how to create text files on an SD card using the FatFS middleware component and FreeRTOS. The application is working on STM32H743I-EVAL board.

 

If your question is answered, please close this topic by clicking "Accept as Solution".

If your question is answered, please close this topic by clicking "Accept as Solution".

Thanks
Omar