2024-02-22 8:36 AM
Hi,
I am using the HAL function "HAL_UARTEx_ReceiveToIdle_DMA" as follows:
void HAL_UARTEx_ReceiveToIdle_DMA(UART_HandleTypeDef *huart, uint16_t Size) {
//my actions
HAL_UARTEx_ReceiveToIdle_DMA(peripheral, buffer, COMMAND_MAXIMUM_LENGTH);
__HAL_DMA_DISABLE_IT(peripheral_dma, DMA_IT_HT);
}
It always works fine after I power up the MCU. I was continuously sending UART frames from my computer to the MCU for 2 days and it worked fine. The idle interruption was always detected.
But when I stop sending frames and then start sending them again (by disconnecting and reconnecting the TX wire), the IDLE interruption is no longer detected… until I turn off and power up the MCU again.
Why?
2024-02-22 8:43 AM - edited 2024-02-22 8:45 AM
Probably a bug in your code. Debug the code, pause, and examine the state of the software state machine in huart. Also look for error flags in the UART registers.
> by disconnecting and reconnecting the TX wire
So the TX line floats? Perhaps triggering a frame error. Do you check for and clear those?
2024-02-22 9:36 AM
The UART registers look nice. Indeed, the ‘HAL_UARTEx_ReceiveToIdle_DMA’ returned HAL_OK the last time before disconnecting.
The TX is not floating.
The interrupt just disables itself. This is because if I put this code inside the while(1) loop:
HAL_UARTEx_ReceiveToIdle_DMA(peripheral, buffer, COMMAND_MAXIMUM_LENGTH);
__HAL_DMA_DISABLE_IT(peripheral_dma, DMA_IT_HT);
It works perfectly...
Why interruption is disable itself?
2024-02-22 1:18 PM - edited 2024-02-22 1:20 PM
> Why interruption is disable itself?
It doesn't. Some code somewhere is disabling it. Do you have an error callback function - HAL_UART_ErrorCallback()? You should. That will show you if you get errors as mentioned by @TDK
EDIT: The HAL UART code will disable the UART (and interrupts) when it detects an error. That error callback it the way you detect that this has happened
2024-02-22 2:27 PM
> The UART registers look nice.
What does this even mean? "Nice" is not objective. Show them, do they indicate an error, do they indicate a transfer in progress? Show the contents of the huart structure. Same questions.
Likely this mystery could be solved within a few minutes of looking into those structures when the problem happens.
2024-02-23 1:00 AM
When I say that I disconnect the transmission, it means that I am disconnecting the wire. All the frames I see on my logic analyzer and oscilloscope are correct, with no glitches or noise.
However, you are right. When I disconnect, my code enters the function HAL_UART_ErrorCallback() and displays sometimes:
HAL_UART_ERROR_FE 0x00000004U /*!< Frame error */.
and other times:
HAL_UART_ERROR_DMA 0x00000010U /*!< DMA transfer error */
I don’t know what causes that error, because it always happens, even sometimes when I disconnect while no frames are being transmitted.
Okay, thank you. I didn’t know about that ErrorCall function. I was debugging by looking at the Huart structure, but since I always stop inside my code, the error code was always correct.
Thank you very much
2024-02-23 6:39 AM
If a frame error is being flagged, the data is likely not as glitchless and noise-free as you are interpreting. Note that a logic analyzer typically may only interpret based on edges.
2024-02-23 2:25 PM
What @TDK said. When you disconnect the wire, does the RX line into the STM32 go low? That would definitely cause a framing error (which means the line is still low at the "stop" bit, i.e. 9.5 bit times after the "start" bit or initial falling edge).