2019-09-01 10:37 AM
Hello,
The short story:
I observe difference in behavior between osDelay() compared to IAR debugger steps.
Is there anything which can explain why these two behaves differently ?
The long story:
Recently we changes our FPGA from asynchronous to synchroous + wait delay + different timing.
Now we observe some issues when accessing FPGA .
We test it as following:
while(1){
wr_value++;
HAL_SRAM_Write_32b(&g_hfpga, FPGA_BANK_ADDR + wr_offset, &wr_value, 1);
HAL_SRAM_Write_32b(&g_hfpga, FPGA_BANK_ADDR + rd_offset, &rd_value, 1);
}Trying to do steps, I see that the rd_value is not always equal to wr_value, and seems to be related to previous values sometimes.
If I only add osDelay between write/read then I always get the correct values:
while(1){
wr_value++;
HAL_SRAM_Write_32b(&g_hfpga, FPGA_BANK_ADDR + wr_offset, &wr_value, 1);
osDelay(125)
HAL_SRAM_Write_32b(&g_hfpga, FPGA_BANK_ADDR + rd_offset, &rd_value, 1);
}Is there anything which can explain the change in behavior between osDelay vs doing steps with debugger ?
Thanks
2019-09-01 12:12 PM
> Is there anything which can explain the change in behavior between osDelay vs doing steps with debugger ?
osDelay may cause task switch, this is pretty heavy and involved procedure.
Also, if your debugger supports RTOS integration, it can do something "clever" and add to the complexity.
-- pa