cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_PCD_EP_Open without HAL_PCD_EP_Receive can result in a hard fault

Tim Schuerewegen
Associate

The HAL_PCD_EP_Open function configures an out endpoint so that the host can actually write data to it, which is kind of a problem because if you did not use HAL_PCD_EP_Receive then ep->xfer_buff is NULL and USB_ReadPMA will generate a hard fault :(

To fix it I changed

PCD_SET_EP_RX_STATUS(USBx, ep->num, USB_EP_RX_VALID);

to

PCD_SET_EP_RX_STATUS(USBx, ep->num, USB_EP_RX_NAK); // was USB_EP_RX_VALID

in

HAL_StatusTypeDef USB_ActivateEndpoint(USB_TypeDef *USBx, USB_EPTypeDef *ep)

I am using STM32Cube_FW_F1_V1.8.0.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0